Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design PicoZed / Carrier Ethernet PHY RXC Routing
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 358 subscribers
  • Views 1548 views
  • Users 0 members are here
Related

PicoZed / Carrier Ethernet PHY RXC Routing

chailatte
chailatte over 11 years ago

Hi folks,


Thinking I've encountered a concern regarding the routing of the Rx Clock on the Ethernet PHY on the PicoZed FMCC Carrier Card, and wanting to turn it over to some other eyes to confirm or refute.


I'm preparing to use the Carrier Card to prototype a gigabit ethernet connection driven by logic on the Zynq PL of a PicoZed card, instantiating the AXI Ethernet Block (R6.2).  (Need to support jumbo frames, which precludes using a MAC of the PS.)


From the schematics of PicoZed and FMCC carrier, I trace the RXC receive channel clock of the Marvell PHY on the carrier through JX2 pin 94 to pad V11 of the Zynq 7020.  But since V11 is not an MRCC or SRCC pin, Vivado (rightfully, I believe) complains vociferously at its inability to successfully route the design.


On further study of the schematics, I find the a nearby JX2 connector pin 74, which does route to an SRCC pin, in the same I/O bank 13 as the other signals of the PHY interface.  It is labeled IO_L14P_T2_SRCC_13 on the Zynq, bonded to pad Y9, and makes the implementation tools much much happier.


But before I turn the carrier card over to our tech folks for the minor surgery needed to reroute the PHY's RXC output through JX2.74, I thought I'd check with the group to see if anyone could confirm (or otherwise comment upon) both:
1) my reading of the documentation; and
2) its accuracy.


In case it matters, the carrier card I have is labeled MBCC-PZCC-PCB-C, 1450043.


Many thanks,


Joseph

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    We are experiencing similar timing problems due to the RX clock pin assignment, when using the GMII to RGMII IP.

    In addition the latest PicoZed Carrier constraints file (Apr 2nd) sets Bank 13 to LVCMOS33. 3V3 is not a supported RGMII voltage signal level for Xilinx 7 series devices. See Table 4-1 on page 42 of the GMII to RGMII v3.0 (PG160) data sheet.

    http://www.xilinx.com/support/documentation/ip_documentation/gmii_to_rgmii/v3_0/pg160-gmii-to-rgmii.pdf

    Bryan: Is there an example available which successfully routes both PS Ethernet ports to the PicoZed carrier?

    Thanks,
    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    We are experiencing similar timing problems due to the RX clock pin assignment, when using the GMII to RGMII IP.

    In addition the latest PicoZed Carrier constraints file (Apr 2nd) sets Bank 13 to LVCMOS33. 3V3 is not a supported RGMII voltage signal level for Xilinx 7 series devices. See Table 4-1 on page 42 of the GMII to RGMII v3.0 (PG160) data sheet.

    http://www.xilinx.com/support/documentation/ip_documentation/gmii_to_rgmii/v3_0/pg160-gmii-to-rgmii.pdf

    Bryan: Is there an example available which successfully routes both PS Ethernet ports to the PicoZed carrier?

    Thanks,
    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • bhfletcher
    0 bhfletcher over 11 years ago in reply to e14 Contributor

    The RGMII using a 3.3V bank is one of the things listed in the Errata that we just posted. You are correct that it is outside the specification provided by Xilinx. I am working on getting a better explanation from Xilinx as to why that requirement exists. In spite of this, we have tested this 2nd Ethernet port with sustained data rates of 800 Mbps.

    We are working on a dual Ethernet example, but we are still several weeks away from having that ready. You may be able to get some assistance from your local Avnet FAE.

    Bryan