Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design PicoZed 7020 QSPI boot problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 358 subscribers
  • Views 1234 views
  • Users 0 members are here
Related

PicoZed 7020 QSPI boot problem

e14 Contributor
e14 Contributor over 10 years ago

Hi,

I have PicoZed 7020 and connected it to the carrier bord. I wrote a simple bare-metal application which sends data from UART port and toggle PS user led pin according to the state of the PS user push button.

When I run the code from JTAG no problem, works correctly. Then I create boot image and download the .mcs file to the flash. I changed boot switchs to qspi flash boot. However when I give the power to the board, blue led turns on as expected, but the program did not run. Dont send data to UART port or toggle user led when I push the user button.

I created MicroZed version of the project and it boots and run correctly from qspi flash. But I was not able to do the same with PicoZed board.

I tried different PicoZed boards and programs. None of them run correctly.

Is there sth. different in PicoZed QSPI flash boot procedure than the MicroZed?

Thanks in advance,

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Problem solved. The exact solution is the one I mentioned before. After I connect SDIO1_SDN to GND, QSPI boot work. Thank you for responses.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Problem solved. The exact solution is the one I mentioned before. After I connect SDIO1_SDN to GND, QSPI boot work. Thank you for responses.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • qyl_qiyalu
    0 qyl_qiyalu over 9 years ago in reply to e14 Contributor

    Hi,

    I have the same problem. connect SDIO1_SDN to GND, what dose SDIO1_SDN mean? I can not find the Pin, Please help me!

    Thank you very much 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 9 years ago in reply to qyl_qiyalu

    I think SDN was a typo. Should have been CDN, which is Card Detect. SDIO1 is connected to eMMC, so that should have no bearing on whether the QSPI will boot, unless you have specifically set up the QSPI to pull a boot image from eMMC.

     

    Connecting the SDIO1 controller's CDN pin to GND to simulate a physical Card Detect was a workaround required prior to 2015.2. Since that time, it is no longer required for booting Linux.

     

    Bryan