Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design pg module led
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 359 subscribers
  • Views 1724 views
  • Users 0 members are here
Related

pg module led

tseong
tseong over 9 years ago

hi.

board : pized 7020 SOM+FMC Carrier v1

originally pg module green led light on.

but, pg module led off.

What should I do with it?

What's wrong?

 

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • jj1989
    jj1989 over 9 years ago +1
    Only your green led light is not working? Could you give more details , please?
  • jafoste4
    jafoste4 over 9 years ago +1
    Hello Tseong, Could you please provide more information. Under what cirumstance is the led ligh on and then off? Was it initially working, and now after some time it has stopped working? PG Module acts…
  • jafoste4
    jafoste4 over 9 years ago +1
    Hello Tseong, I am still a bit confused. So did you populate the con1 connector with an FMC that you are using to monitor the data and clock? Also is your board new strait out of the box and you are having…
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Tseong,

    Could you please provide more information. Under what cirumstance is the led ligh on and then off? Was it initially working, and now after some time it has stopped working? PG Module acts as a handshake between the SOM and the Carrier indicating that the SOM is being powered properly by the Carrier Card.

    So with that being said, check and make sure your SOM is properly connected to you carrier card. Then check and make sure your 12V AC/DC adapter is plugged in propperly(perhaps try a different wall AC port as well). Also does the "FPGA DONE" led light up?  

    Next you can double check you have your Carrier Card setup properly. We have the setup documented on Page 15 of the "Tutorial 02 First Application - Hello World" reference design. You can find it at http://zedboard.org/support/design/13076/106

    --Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Tseong,

    Could you please provide more information. Under what cirumstance is the led ligh on and then off? Was it initially working, and now after some time it has stopped working? PG Module acts as a handshake between the SOM and the Carrier indicating that the SOM is being powered properly by the Carrier Card.

    So with that being said, check and make sure your SOM is properly connected to you carrier card. Then check and make sure your 12V AC/DC adapter is plugged in propperly(perhaps try a different wall AC port as well). Also does the "FPGA DONE" led light up?  

    Next you can double check you have your Carrier Card setup properly. We have the setup documented on Page 15 of the "Tutorial 02 First Application - Hello World" reference design. You can find it at http://zedboard.org/support/design/13076/106

    --Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • tseong
    0 tseong over 9 years ago in reply to jafoste4

    answer, thank you. 

    but, i have board basic setting complete.

    i problem situation, i used to oscilloscope in 'con1' connector. 

    The reason for using the connector is to check the data and clock.

    at any moment vin led ligth is on. other light leds is off.

    please detailed answer. thank you.