Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design SD card DET pin
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 357 subscribers
  • Views 4476 views
  • Users 0 members are here
Related

SD card DET pin

oscargomezf
oscargomezf over 10 years ago

Hi everyone,

I'm working on a new design based on the PicoZed FMC Carrier Card V2. I'm considering using a micro SD card connector without insert card detection signal (DET).

In the schematic of the PicoZed FMC Carrier Card V2 is called SD_CD.

When the SD card detection is activated, the pins G3 and G4 are open and the SD_CD signal is high due to the pull-up resistor R68. If the SD card isn't inserted then the pins G3 and G4 are close and the SD_CD signal is GND.

What do I have to consider in the design?

Do I have to place a pull-up resistor to simulate that the SD card is always inserted?

Obviously, I only could insert the SD card when the system is power off. But It's not always going te be inserted an SD card.

 

Best regards.

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    I'm not quite sure what you are trying to do.  You first mention that you want to not use the DET pin.  Then you go on to mention a few things that makes me think that you will sometimes have the memory there and sometimes not.

    Can I first ask, why don't you want to use the pin?

    You can certainly use pull-up or pull-down to set various states, however, you will be limiting what your system can do.  I would also like to point out that I am not aware of any SD Card cage that does not provide the appropriate signaling, which is why I asked above why you do not want to use that signal.  You make it seem that you ARE going to use an SD card cage, so this is confusing to me.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    I'm not quite sure what you are trying to do.  You first mention that you want to not use the DET pin.  Then you go on to mention a few things that makes me think that you will sometimes have the memory there and sometimes not.

    Can I first ask, why don't you want to use the pin?

    You can certainly use pull-up or pull-down to set various states, however, you will be limiting what your system can do.  I would also like to point out that I am not aware of any SD Card cage that does not provide the appropriate signaling, which is why I asked above why you do not want to use that signal.  You make it seem that you ARE going to use an SD card cage, so this is confusing to me.

    --Dan