Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design RTC for Picozed?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 1127 views
  • Users 0 members are here
Related

RTC for Picozed?

e14 Contributor
e14 Contributor over 11 years ago

Does the Picozed board include a real time clock, or is one built into the Zynq?

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 11 years ago

    Hi kadatech,

    I assume by RTC you are talking about a calendar timekeeping device like you find on some of the other eval boards.  The answer is that Zynq has some hardware timers but it does not have a calender timekeeping feature that I am aware of.

    If you are looking for that type of functionality, it can be added using something like the Maxim DS3231 which comes in a Pmod expansion module that can be added to one of our carrier cards that has Pmod expansion ports available.  Check out the Maxim Analog essentials kit which has this RTC Pmod:

    http://www.maximintegrated.com/en/app-notes/index.mvp/id/5468

    The idea here is that if you need RTC for your application, you would need to build one of these components onto your own PicoZed carrier design.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kemaangu
    0 kemaangu over 8 years ago

    Hi 

    I am using Picozed board . Here are details:

    PicoZed FMC Carrier Card V2 (http://zedboard.org/product/picozed-fmc-carrier-card-v2) 

    SOM as Picozed 7015/7030 ( http://zedboard.org/support/documentation/4736)

    I built the custom Linux kernel (4.9) for using RTC (aim to detect the device file as /dev/rtc0).  From Hardware user guide of carrier card, it is understood that RTC on carrier card is Maxim DS3231 at address 0xD0 which is attached to HDMIO I2C bus and the source lines (HDMIO_SCL, HDMIO_SDA) of HDMIO I2C bus is from ADV7511 (HDMI decoder). I feel this ADV7511 interfaces only with FPGA.  Please confirm, that only through writing PL for FPGA, you can make ADV7511 functional, not from SOM, right? If so, then this the way to enable HDMIO I2C bus for RTC. As said earlier, the  other way of making RTC functional only through PMOD interface.  Please confirm.  

    Thanks & Regards

    Manjunatha Srinivasan N 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Manjunatha,

    Yes you are correct, this is how you make the RTC available. Kevins initial comment was back when only the PicoZed FMC V1 was available. That Carrier Card does not have a RTC available.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kemaangu
    0 kemaangu over 8 years ago in reply to jafoste4

    Hi Josh 

    Thanks for valuable information. Please suggest FPGA for PicoZed FMC Carrier Card V2. 

     Regards

    Manjunatha Srinivasan N