Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Boot Mode Select and Defaults
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 357 subscribers
  • Views 368 views
  • Users 0 members are here
Related

Boot Mode Select and Defaults

Bertl
Bertl over 12 years ago

The "Boot Mode Select" table in the 7015/30 schematic (rev B2) has some errors, i.e. there is no LOW(5-6) for JT2 and I also presume that the first SW1 column should read LOW(2-3) instead of LOW(5-6).

Assuming that JT2 is really meant there and not JT4, then the default for JT2 is LOW(1-2).
Note that there also would be no HIGH(1-2) or LOW(2-3) for JT4, as 1 is connected to GND and 3 to VCC in both cases.

But now to the real question here:
What are the BOOT modes selectable via SW1 without changing any of the default SMD solder jumpers JT1-JT4?

Thanks in advance,
Herbert

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    You are correct, there is an error. Thanks for letting us know.

     

    The table column 2 header should read "JT4" instead of JT2. We will correct this and repost.

     

    JT1-JT3 do not play any role in boot mode selection, only JT4 and SW1.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    You are correct, there is an error. Thanks for letting us know.

     

    The table column 2 header should read "JT4" instead of JT2. We will correct this and repost.

     

    JT1-JT3 do not play any role in boot mode selection, only JT4 and SW1.

     

    -Gary