Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design PicoZed Flash Upgrade
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 359 subscribers
  • Views 1184 views
  • Users 0 members are here
Related

PicoZed Flash Upgrade

bhfletcher
bhfletcher over 11 years ago

The Flash image for the PicoZed SOMs that ships from the factory has been updated. All SOMs manufactured after 15 June 2015 will have the new image. Advantages of the new upgrade include:

  •   Update to PetaLinux 2014.4, which eliminates some Ethernet performance issues present in earlier kernels
  •   Uses QSPI for bitstream, FSBL, and U-boot with eMMC to hold the kernel image
  •   Includes fix to Linux kernel which occasionally caused the eMMC to hang
  •   Scripted to allow the user to bypass the Avnet Factory Test which requires extra loopback devices and connectors
  •   Corrects previous 7015 and 7030 failures to load the bitstream and boot past U-boot into Linux
  •   The MTD partitions are now consistent across all PicoZed variants, which means for the factory test we can use the same image.ub file for every device.
  •   Adds e4fsprogs package to allow ext4 formatting of eMMC
  •   eMMC is dual partitioned with a 128 MB FAT partition (to hold the Linux kernel) and a 3.3 GB ext4 partition for user space

 

http://picozed.org/support/design/4701/76 

Restore/Upgrade QSPI Factory Image

Use this document and archive along with your PicoZed and PicoZed FMC Carrier Card to restore or upgrade the factory test image to the QSPI and eMMC on the PicoZed.

Restore QSPI Factory Image (12 Jun 15)

 

With the updated Factory Image, please refer to PicoZed FMC Carrier Card Getting Started Guide v2.1 (for use with 12 Jun 15 firmware) for instructions.

http://picozed.org/support/documentation/4701

 

Bryan

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 11 years ago

    Hi Joe,

     

    I asked our manufacturing team, and they tell me that they have not yet initiated a build with the new Flash image. I have asked them to monitor the serial numbers so that I can replay back here when that happens.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 11 years ago

    Hi Joe,

     

    I asked our manufacturing team, and they tell me that they have not yet initiated a build with the new Flash image. I have asked them to monitor the serial numbers so that I can replay back here when that happens.

     

    Bryan