Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design FMC V1 Power
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 358 subscribers
  • Views 534 views
  • Users 0 members are here
Related

FMC V1 Power

e14 Contributor
e14 Contributor over 10 years ago

Hi,

   FMC V1 - PCIe power question.

  Is it ok to have the main power supply (via J14) connected when the board is installed in a PC.

 Both J14 and the PCIe connector will be providing a 12V supply. 

 D22/23 seem to provide isolation but I'm just being

super cautious.

Regards,

   Elwyn

  • Sign in to reply
  • Cancel
Parents
  • ctammann
    0 ctammann over 9 years ago

    Hi Elwyn,

     

    Does the PC you are using have a spec compliant PCIe slot?  The reason I ask is if I'm not mistaken the PCIe spec states that the interface can provide up to 75W.  The PicoZed and carrier should draw nowhere near that.  I'd expect less than 8W, realistically around 5W or less.  That being said, perhaps you are running into an inrush limiting situation where the supply is going into overcurrent at startup.  Can you look at the startup and see if when the supply starts ramping that it starts smoothly and doesn't glitch or turn off?  I would look at the 12V feeding the FMC carrier.  That should at least tell us if the FMC load is impacting boot up.

    Thanks

    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ctammann
    0 ctammann over 9 years ago

    Hi Elwyn,

     

    Does the PC you are using have a spec compliant PCIe slot?  The reason I ask is if I'm not mistaken the PCIe spec states that the interface can provide up to 75W.  The PicoZed and carrier should draw nowhere near that.  I'd expect less than 8W, realistically around 5W or less.  That being said, perhaps you are running into an inrush limiting situation where the supply is going into overcurrent at startup.  Can you look at the startup and see if when the supply starts ramping that it starts smoothly and doesn't glitch or turn off?  I would look at the 12V feeding the FMC carrier.  That should at least tell us if the FMC load is impacting boot up.

    Thanks

    Chris