Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Accessing PicoZed 7030 eMMC in u-boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 358 subscribers
  • Views 1145 views
  • Users 0 members are here
Related

Accessing PicoZed 7030 eMMC in u-boot

nitsch
nitsch over 8 years ago

We are using PicoZed 7030 on a FMCv2 carrier board. Running a custom Linux from SD card, we can access both the SD card as well as the on-board eMMC (after explicitly enabling sdhci1 in the device tree). In u-boot, however, the only available mmc device is the SD card. What is necessary to also access eMMC in u-boot?

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 8 years ago

    Hi nitsch,

    I have only had experience accessing one or the other (SD card or eMMC) from U-boot since usually having both are not needed in an end application though potentially useful during development.

    You may need to dig into the U-Boot source to find out an answer to your question but I have seen this recently come across where it appears that updates from the SD card to eMMC contents are possible once you declare the second SDHCI controller in platform-top.h header:

    https://github.com/Avnet/petalinux/blob/master/configs/u-boot/platform-top.h.pz_emmc_boot

    Perhaps something similar would work for your application?

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nitsch
    0 nitsch over 8 years ago in reply to zedhed

    We tried enabling only one of the MMC devices, but the SD card is the only one that works in u-boot. The one for the eMMC is never listed. So it currently is either SD card or nothing.

    Thanks for the link. We are not using Petalinux but we will have a look at what they might be doing differently from a vanilla Xilinx u-boot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • nitsch
    0 nitsch over 8 years ago in reply to zedhed

    We tried enabling only one of the MMC devices, but the SD card is the only one that works in u-boot. The one for the eMMC is never listed. So it currently is either SD card or nothing.

    Thanks for the link. We are not using Petalinux but we will have a look at what they might be doing differently from a vanilla Xilinx u-boot.