Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Accessing PicoZed 7030 eMMC in u-boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 358 subscribers
  • Views 1147 views
  • Users 0 members are here
Related

Accessing PicoZed 7030 eMMC in u-boot

nitsch
nitsch over 8 years ago

We are using PicoZed 7030 on a FMCv2 carrier board. Running a custom Linux from SD card, we can access both the SD card as well as the on-board eMMC (after explicitly enabling sdhci1 in the device tree). In u-boot, however, the only available mmc device is the SD card. What is necessary to also access eMMC in u-boot?

  • Sign in to reply
  • Cancel
Parents
  • nitsch
    0 nitsch over 8 years ago

    We fixed it. It was an oversight on our part. Sorry for the noise.

    When building the u-boot, make sure to use the picozed defconfig, not the zed defconfig. Duh.

    The u-boot uses its own set of device tree files, apparently built into the u-boot image. Sources for these files are found in arch/arm/dts/. The one for zed only enables sdhci0 (the SD card) but not sdhci1 (the eMMC). This explains the behaviour we were observing. The dts for picozed only enables the latter by Default, which makes the eMMC work. Editing the dts to enable sdhci0 and sdhci1 makes it possible to access both SD card and eMMC in u-boot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • nitsch
    0 nitsch over 8 years ago

    We fixed it. It was an oversight on our part. Sorry for the noise.

    When building the u-boot, make sure to use the picozed defconfig, not the zed defconfig. Duh.

    The u-boot uses its own set of device tree files, apparently built into the u-boot image. Sources for these files are found in arch/arm/dts/. The one for zed only enables sdhci0 (the SD card) but not sdhci1 (the eMMC). This explains the behaviour we were observing. The dts for picozed only enables the latter by Default, which makes the eMMC work. Editing the dts to enable sdhci0 and sdhci1 makes it possible to access both SD card and eMMC in u-boot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer