Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Differences between PicoZed 7Z030 REVC01 and REVC04
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Subscribers 358 subscribers
  • Views 1593 views
  • Users 0 members are here
Related

Differences between PicoZed 7Z030 REVC01 and REVC04

e14 Contributor
e14 Contributor over 9 years ago

I have a custom PicoZed carrier board. The PicoZeds that I have been using with it are labeled BD-Z7PZP-7Z030-G REVC01. These have been working. I just received a new batch of PicoZeds labeled BD-Z7PZP-7Z030-G REVC04.

When I plug these new pz boards into my carrier, set them to cascaded JTAG boot mode, and power them up, I get green power good lights on both the pz and my carrier. Then, after a second or so, I see the blue FPGA_DONE light on my carrier light up. At this point, I don't expect the FPGA to have been configured, as it is in JTAG mode. Furthermore, I can not see the device on the JTAG chain.

Are there any differences between the two revisions of the boards that may be causing this? I've already tried changing the position of JT2 to match the PUDC settings of REVC01. This had no effect. 

One more data point to confuse things: When I plug the new picozeds into my Avent FMC Carrier Card Rev C, the boards work as expected.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    This issue has been resolved. Pulldown resistors at the reset buttons on my carrier had been marked DNI, but were populated. This left CARRIER and POR resets in states somewhere between high and low logic. I was just getting lucky with the REVC01 picozeds.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    This issue has been resolved. Pulldown resistors at the reset buttons on my carrier had been marked DNI, but were populated. This left CARRIER and POR resets in states somewhere between high and low logic. I was just getting lucky with the REVC01 picozeds.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer