Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design USB UART in PicoZed FMC Carrier Card V2
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 357 subscribers
  • Views 554 views
  • Users 0 members are here
Related

USB UART in PicoZed FMC Carrier Card V2

oscargomezf
oscargomezf over 10 years ago

Hi,

 

I'm working on a new project based on the PicoZed and PicoZed FMC Carrier Card V2. I'm going to design a custom Carrier Card.

 

I'm trying to  understand the schematics and I have some doubts related to USB UART.

 

I don't understand, Why do they use a level shifter on the USB_UART_TXD and USB_UART_RXD with a p-mos BSS138?

 

I think it's a better option to eliminate the two bss-138 p-mos and connected them  (USB_UART_TXD  & USB_UART_RXD) directly, and feed the pin 5 (VIO) of the CP2104 IC to 1.8 Volts.

 

Does anyone know if I'm right?

 

Best regards.

  • Sign in to reply
  • Cancel

Top Replies

  • bhfletcher
    bhfletcher over 10 years ago +1 verified
    The CP2104 has issues when you attempt any self-powering. The circuit must be 100% bus-powered or you must design in extra protection circuitry. This is our 3rd time using the CP2104, and we learned some…
Parents
  • bhfletcher
    0 bhfletcher over 10 years ago

    The CP2104 has issues when you attempt any self-powering. The circuit must be 100% bus-powered or you must design in extra protection circuitry. This is our 3rd time using the CP2104, and we learned some of these lessons the hard way. Check out the Errata for MicroZed and the FMC-V1 for details.

     

    What you propose mixes a self-powered VIO while the rest of the circuit is bus-powered. If VIO were connected to the on-board 1.8V, here is the issue:

    1.   VIO is connected to net 1.8V
    2.   Q1 and Q2 are removed to allow a direct connection between CP2104 and Zynq
    3.   CP2104 RSTn (pin 9) is pulled-up to VIO
    4.   You plug in the USB cable prior to powering on the board
    5.   You then power on the board
    6.   The USB-UART does not enumerate in some cases

    For an explanation why, see http://microzed.org/content/usb-uart-pzcc-fmc-wont-enumerate

     

    According to the datasheet, the RSTn pin may also be an open-drain POR status. However, from what we heard from SiLabs, the RSTn circuit is powered internally by VIO, which is why the circuit examples show pulling it up to VIO. We worried that leaving RSTn floating with VIO unpowered would also cause issues in some cases.

     

    We considered adding a small 1.8V regulator sourced by CP2104 VDD. The level translator option that we used was cheaper.

     

    As the circuit is now, the CP2104 will consistently enumerate as soon as the cable is plugged in, regardless of whether board power is on or not.

     

    Bryan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • oscargomezf
    0 oscargomezf over 10 years ago in reply to bhfletcher

    Thank you very much for you explanation.

     

    Now I understand everything and I'm calm because I understand why it's made the design of this way.

     

    Best regards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • oscargomezf
    0 oscargomezf over 10 years ago in reply to bhfletcher

    Thank you very much for you explanation.

     

    Now I understand everything and I'm calm because I understand why it's made the design of this way.

     

    Best regards.