Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design VCCO_34/35 limitation between 7010/20 and 7015/30
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 356 subscribers
  • Views 274 views
  • Users 0 members are here
Related

VCCO_34/35 limitation between 7010/20 and 7015/30

bhfletcher
bhfletcher over 11 years ago

When the PicoZed 7015/30 PCB was designed, it made more sense to rotate the Zynq device 180 degrees in comparison to the 7010/20 PCB. This allowed for easier transceiver routing from the 7015/30 Zynq device to JX3. With the rotation, it also made more sense to put the Bank 35 I/Os on JX1 and the Bank 34 I/Os on JX2.

 

Although the Bank 34 and 35 I/Os were exchanged on JX1/JX2, the VCCO pins were not. This leads to a limitation if you plan to design a carrier that supports multiple members of the PicoZed family:

  •   If the Carrier has different voltages on VCCO_34 and VCCO_35, then
  •   the Carrier cannot migrate between the 7010/20 and 7015/30. Only one family pair can be supported.

Avnet's PicoZed FMC Carrier shares the same voltage on VCCO_34 and VCCO_35, therefore, it can support any of the SOMs.

If you only plan to migrate between the 7010 and 7020 or the 7015 and 7030, then you will also not have this limitation.

 

Bryan

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 11 years ago

    One more distinction on compatibility between a Carrier designed to support BOTH the 7015 and 7030 -- VCCO_34 and VCCO_35 must both be 1.8V or lower since Banks 34 and 35 are both HP banks on the Zynq 7030.

     

    Bryan