Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design XADC VP VN pin
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 357 subscribers
  • Views 852 views
  • Users 0 members are here
Related

XADC VP VN pin

marcomercuri85
marcomercuri85 over 9 years ago

Hi all,

I would like to use the internal XADC. Looking at the schematic, it seems that the PicoZed FMC Carrier Card V2 does not support connections to the VP/VN analog input (JX1.97, JX1.98, JX1.99, JX1.100). Is it that true?

If yes, what should I do to use the XADC? If not, where I can find these pins on the carrier card?

Thanks.

Best Regards,

Marco 

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 9 years ago

    Hi there,

    Which SOM are you intending to use?
    Ball F7 is a GROUND on a 7010 based SOM.
    On a 7030, that ball is marked as a AD0P for XADC, which means you could use that.  That signal will end up on the FMC LPC connector.

    Again, depending on your accuracy requirements (Eb/No), due to this signal being routed for DIGITAL not ANALOG on the FMCv2, as well as the amount of support out there, I would again recommend you use an ADC on a PMOD instead of using this pin.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drozwood90
    0 drozwood90 over 9 years ago

    Hi there,

    Which SOM are you intending to use?
    Ball F7 is a GROUND on a 7010 based SOM.
    On a 7030, that ball is marked as a AD0P for XADC, which means you could use that.  That signal will end up on the FMC LPC connector.

    Again, depending on your accuracy requirements (Eb/No), due to this signal being routed for DIGITAL not ANALOG on the FMCv2, as well as the amount of support out there, I would again recommend you use an ADC on a PMOD instead of using this pin.

    --Dan