Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Micron eMMC meets Xilinx requirement
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 357 subscribers
  • Views 2105 views
  • Users 0 members are here
Related

Micron eMMC meets Xilinx requirement

bhfletcher
bhfletcher over 11 years ago

PicoZed is populated with a Micron 4GB, v4.41 MTFC4GMDEA-4M IT eMMC device.

http://www.micron.com/parts/nand-flash/managed-nand/mtfc4gmdea-4m-it

 

Xilinx has a Design Advisory related to eMMC and performance: http://www.xilinx.com/support/answers/59999.html. Essentially, it states that the Zynq-7000 SDIO Controller operated in High Speed Mode is NOT compliant with the JEDEC standard 4.41 for eMMC.  The only way you can run in High Speed Mode (50 MHz) is to add tuning to your board traces or verify with the eMMC manufacturer that the characterized hold time is 2ns or less.

 

Avnet has verified with Micron that the characterized hold time for MTFC4GMDEA-4M IT is well under 2ns.  In other words, though the 2ns is outside JEDEC standard specifications, the Micron eMMC can still comply and function with the Zynq-7000 host SDIO controller in High Speed Mode.

 

This specific characterization data may be obtained under NDA with Micron.

 

Bryan

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi Bryan, it seems that the Micron part you mention is obsolete; Which replacement would you recommend?

    BTW, do you know of a 64GB (or larger than 4GB) device verified with Zynq?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 10 years ago in reply to e14 Contributor

    According to Micron, the MTFC4GMDEA-4M IT is in production currently, but not recommended for new designs.  EOL is estimated for end of 2017, so we have some time yet, especially when you consider that we could do a last-time buy.

     

    That said, we will likely qualify a v5.0 eMMC sometime during the Fall of this year. When we do that, we will issue a PCN to inform customers of this change. If you have a requirement to have PicoZeds with the exact current component list, then you should work with your Avnet sales office to get that on order with your specific requirements.

     

    For the current device, there is an 8GB version that should work, but we have not qualified it previously -- MTFC8GLDEA-4M IT.

     

    For the future device (MTFC4GACAJCN-4M IT) that we are considering, the family density ranges from 4GB to 64GB. 

     

    If you have a requirement for a larger eMMC, please contact your local Avnet sales office or customize@avnet.com.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 9 years ago in reply to bhfletcher

    I can confirm that we have validated the v5.0 eMMC with Zynq-7000 on all of our PicoZed platforms as well as the 7Z007S on MiniZed. All MiniZed and all future PicoZed will be built with Micron MTFC8GAKAJCN-4M IT.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 9 years ago in reply to bhfletcher

    I can confirm that we have validated the v5.0 eMMC with Zynq-7000 on all of our PicoZed platforms as well as the 7Z007S on MiniZed. All MiniZed and all future PicoZed will be built with Micron MTFC8GAKAJCN-4M IT.

    Bryan