Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design AXI UART causes petalinux-build to fail
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 360 subscribers
  • Views 792 views
  • Users 0 members are here
Related

AXI UART causes petalinux-build to fail

100jthilliard
100jthilliard over 8 years ago

I have added an AXI UART in Vivado to the standard P7Z30 with FMC carrier V2 design. However, when I select this UART as the primary stdin/stdout, petalinux-build fails during the do-compile. What else do I need to do in order to make this UART usable?

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    When you say it fails during compilation, what errors are you getting?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100jthilliard
    0 100jthilliard over 8 years ago

    It gives error 1, which is the catch-all error for linux. The detailed error message it gives is a long filepath that basically says that do-compile failed while compiling the AXI UART. I will try to find the full filepath and post it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100jthilliard
    0 100jthilliard over 8 years ago

    The full text of the error reads: 

    ERROR: Task (/home/aces/Documents/petalinux/components/yocto/source/arm/layers/meta-xilinx/recipes-bsp/u-boot-xlnx_2017.01.bb:do_compile) failed with exit code '1'

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 8 years ago

    Hi jthilliard,

    Looking at UG1144, I see the following related to settings for stdin/stdout:

    Ensure the PetaLinux project is built with the right hardware platform.
    u00B0 Import hardware configuration properly, refer to section Import Hardware Configuration.
    u00B0 Check the "Subsystem AUTO Hardware Settings --->" submenu to ensure it matches the hardware platform.
    u00B0 Check the "Serial settings --->" submenu under "Subsystem AUTO Hardware Settings --->" to ensure stdout, stdin are set to the correct UART IP core.
    u00B0 Rebuild system images, see Build System Image.

    Source:

    https://www.xilinx.com/support/documentation/sw_manuals/xilinx2017_4/ug1144-petalinux-tools-reference-guide.pdf

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago in reply to 100jthilliard

    Have you included all of the dependencies? In the Serial Settings menu, pressing 'h' will show the dependencies for your selected stdin/stdout option.