Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design PicoZed fails to load OS from eMMC at low temp
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 1150 views
  • Users 0 members are here
Related

PicoZed fails to load OS from eMMC at low temp

e14 Contributor
e14 Contributor over 10 years ago

I am using the  AES-Z7PZ-7Z015-SOM-G Rev C04. When the board is cold started (power up after being powered off for a while) it will boot into Pentalinux but will not load the OS from the eMMC. After a couple of power cycles it will eventually boot al the way up.  

I put the SOM and Carrier in a temperature chamber and I could repeat the failure when the set point was less than 20C.

Below is a log of what I am seeing when it fails:

 

U-Boot 2015.07 (Sep 01 2016 - 14:31:20 -0500)

 
DRAM:  ECC disabled 1 GiB
MMC:   zynq_sdhci: 0
SF: Detected S25FL128S_64K with page size 256 Bytes, erase size 64 KiB, total 16 MiB
In:    serial
Out:   serial
Err:   serial
Net:   Gem.e000b000
Hit any key to stop autoboot:  4  3  2  1  0 
sdhci_transfer_data: Error detected in status(0x208000)!
Device: zynq_sdhci
Manufacturer ID: fe
OEM: 14e
Name: MMC04
Tran Speed: 52000000
Rd Block Len: 512
MMC version 4.4.1
High Capacity: Yes
Capacity: 3.5 GiB
Bus Width: 4-bit
Erase Group Size: 512 KiB
HC WP Group Size: 4 MiB
User Capacity: 3.5 GiB
Boot Capacity: 16 MiB ENH
RPMB Capacity: 128 KiB ENH
** Unrecognized filesystem type **
U-Boot-PetaLinux> 
  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 10 years ago

    We tested PicoZed well below +20C. The C-grade version was tested down to -25C and the I-grade down to -45C. I would like to try and duplicate this issue here on my bench. Is this a problem that you can duplicate with an Avnet Carrier and the pre-built image that we have posted for PetaLinux? If so, I will try the same thing.

    http://picozed.org/support/design/4701/76 

      PetaLinux 2015.4 Compressed BSP, z7015

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bhfletcher

    I have 5 SOM and we have seen this issue on 2 of the 5.  I can try reverting back to the pre-built image and will post the results.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bhfletcher

    I have 5 SOM and we have seen this issue on 2 of the 5.  I can try reverting back to the pre-built image and will post the results.