Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design PicoZed fails to load OS from eMMC at low temp
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 1150 views
  • Users 0 members are here
Related

PicoZed fails to load OS from eMMC at low temp

e14 Contributor
e14 Contributor over 10 years ago

I am using the  AES-Z7PZ-7Z015-SOM-G Rev C04. When the board is cold started (power up after being powered off for a while) it will boot into Pentalinux but will not load the OS from the eMMC. After a couple of power cycles it will eventually boot al the way up.  

I put the SOM and Carrier in a temperature chamber and I could repeat the failure when the set point was less than 20C.

Below is a log of what I am seeing when it fails:

 

U-Boot 2015.07 (Sep 01 2016 - 14:31:20 -0500)

 
DRAM:  ECC disabled 1 GiB
MMC:   zynq_sdhci: 0
SF: Detected S25FL128S_64K with page size 256 Bytes, erase size 64 KiB, total 16 MiB
In:    serial
Out:   serial
Err:   serial
Net:   Gem.e000b000
Hit any key to stop autoboot:  4  3  2  1  0 
sdhci_transfer_data: Error detected in status(0x208000)!
Device: zynq_sdhci
Manufacturer ID: fe
OEM: 14e
Name: MMC04
Tran Speed: 52000000
Rd Block Len: 512
MMC version 4.4.1
High Capacity: Yes
Capacity: 3.5 GiB
Bus Width: 4-bit
Erase Group Size: 512 KiB
HC WP Group Size: 4 MiB
User Capacity: 3.5 GiB
Boot Capacity: 16 MiB ENH
RPMB Capacity: 128 KiB ENH
** Unrecognized filesystem type **
U-Boot-PetaLinux> 
  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 9 years ago

    We've been experimenting with the cold start eMMC issues mentioned above. I can confirm that we have seen this issue after testing enough boards. I estimate that this affects 25% of all PicoZed SOMs.

    We have also found a work-around to eliminate the failure. The solution is to switch the Zynq SDIO clock from the typical high-speed mode to standard-speed mode. While we do not think we have the Hold problem identified in this Design Advisory based on measurements that we have taken, the suggestion to switch to Standard Speed Mode does work.

    http://www.xilinx.com/support/answers/59999.html

     

    We have posted updated copies of the PetaLinux 2016.2 BSPs that puts U-boot and PetaLinux both into SDIO Standard Speed Mode for the eMMC, which uses the Zynq PS SD1 controller on PicoZed. Please check out these updated BSPs, posted on the PicoZed Carrier pages:

    http://picozed.org/support/design/13076/106

     

    http://picozed.org/support/design/4701/76

     

    We will also release an Errata that states that PicoZed does not support High Speed Mode clocking for the eMMC.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 9 years ago

    We've been experimenting with the cold start eMMC issues mentioned above. I can confirm that we have seen this issue after testing enough boards. I estimate that this affects 25% of all PicoZed SOMs.

    We have also found a work-around to eliminate the failure. The solution is to switch the Zynq SDIO clock from the typical high-speed mode to standard-speed mode. While we do not think we have the Hold problem identified in this Design Advisory based on measurements that we have taken, the suggestion to switch to Standard Speed Mode does work.

    http://www.xilinx.com/support/answers/59999.html

     

    We have posted updated copies of the PetaLinux 2016.2 BSPs that puts U-boot and PetaLinux both into SDIO Standard Speed Mode for the eMMC, which uses the Zynq PS SD1 controller on PicoZed. Please check out these updated BSPs, posted on the PicoZed Carrier pages:

    http://picozed.org/support/design/13076/106

     

    http://picozed.org/support/design/4701/76

     

    We will also release an Errata that states that PicoZed does not support High Speed Mode clocking for the eMMC.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer