Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design fmchc_python1300c reference design
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 359 subscribers
  • Views 1633 views
  • Users 0 members are here
Related

fmchc_python1300c reference design

e14 Contributor
e14 Contributor over 8 years ago

Hi,

I am trying to get the fmchc_python1300c reference design to work with Vivado 2016.4

Everything worked fine until I actually wanted to run the demo application on the board.

I used the JTAG cable to run the demo via SDK in with the debugger enabled. The problem I have is, that the program gets stuck in an infinite loop when executing the function "fmc_hdmi_cam_init"

I doesn't get past this point. The system just freezes.

I am using the System Debugger, because the GDB Debugger does not work with the error "no associated elf file".

 

I haven't tried booting from the SD-Card. I will try this and see if the problem also occurs.

 

Has anybody encountered this problem?

 

edit: The vanilla BOOT.bin also gets stuck after ouputting "FMC-HDMI-CAM Initialization ...".

It seems that this is the same behavior...

edit2: I am using the FMC Carrier Card V1. The reference design says that the FMC Carrier Card V2 is required. Is this a problem or is the design compatible with both carrier cards?

I already looked at the pin out of the fmc, and did not see any huge differences that might not make the design work... 

  • Sign in to reply
  • Cancel
  • albertabeef
    0 albertabeef over 8 years ago

    Fynn,

    Please try this version of the design for 2016.4:

       FMCHC_PYTHON1300C_Tutorial_2016_4_01.zip
       https://avnet.egnyte.com/dl/z5PuYyYjG8 

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago in reply to albertabeef

    thank you for your reply. Unfortunately the link is no longer valid. Could you re-upload this version of the design so that I can test it?

     

    Thank you and best regards

    Fynn

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    when I unplug the fmc camera board from the PicoZed Carrrier, the software does not freeze and runs without issues. Unfortunately, this is only a partial solution, since I cannot use the software because the camera is not connected to the fmc.

    So the camera module is basically the problem...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    This issue is still present. I have not been able to download to above link. It is no longer valid, so I cannot confirm if this solution was working or not. Any response would be appreciated

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Fynn,

    I believe this is what you were looking for

    https://avnet.egnyte.com/dl/yL8ZlijBjT

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago in reply to jafoste4

    Hi Josh,

     

    thank you for the upload. This reference design works with the FMC V2 Board but not with the FMC V1 board.

    I had to buy another board to get this design running.

    Do you know if there is a guide on how to make the reference design work on the FMC V1 board?

     

    Best regards

    Fynn

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    Hi again,

     

    the boot process of the reference design seems to work fine. However, I am not able to get an HDMI output onto my monitor. It just stays black and the textbox on the screen says "going to power save mode". I tried it on several monitors... no difference.

    I also tried out the vanilla BOOT.bin, that is also provided with the files and here it is the same problem.

    Is there something that I need to type in the command line for this to work?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago in reply to e14 Contributor

    Hi,

    i have solved now all my problems with this reference design. The reason why I did not get any hdmi ouput on my monitor was because of the R52 resistor on the PicoZed SOM.

    http://zedboard.org/content/picozed-7015-7030-users-action-needed

    After removing R52, the design worked. It might be good to state this somewhere that this could be an issue because I have not identified this required action as mandatory for this design to work.

     

    Best

    Fynn

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jyingling@mobexp.com
    0 jyingling@mobexp.com over 8 years ago in reply to jafoste4

    Hello JFoster,

    The link you provided is no longer available. Can you please provide it again? I cannot find the fmchc_python1300c on github as described in the tutorial: file:///C:/Users/mxadmin/Desktop/MiniMe/tutorials/FMCHC_PYTHON1300C_Tutorial_2016_4_01_0/FMCHC_PYTHON1300C_Tutorial_2016_4_01.pdf

    Thanks in advance.

    -Jeff 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago in reply to jyingling@mobexp.com

    Hello Jeff,

    Here you go

    https://avnet.egnyte.com/dl/Us5DDPFAkN

    --Josh