Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Carrier reference, ADP5052 PWRGD used as PG_MODULE - too early?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 357 subscribers
  • Views 626 views
  • Users 0 members are here
Related

Carrier reference, ADP5052 PWRGD used as PG_MODULE - too early?

e14 Contributor
e14 Contributor over 10 years ago

In the PicoZed PCIe FMC carrier reference design (both V1 and V2), the ADP5052 PWRGD signal is being used as PG_MODULE to signal the Zynq to boot.

From what I can tell from the ADP5052 datasheet, the PWRGD signal is asserted as soon as the channel 1 supply is "good". It doesn't monitor channels 2-4 unless you special order a custom version of the ADP5052, and 5 cannot be monitored.

In V1 of the carrier card, Channel 1 is used for the 1.0V supply, and it is enabled first. I believe that means that the Zynq will start booting up before the other supplies (1.2, 1.8, 3.3) have come up (probably not by much, but technically still before).

In V2 of the carrier card, the channels are used in a different order such that Channel 1 and 2 are the last to come up.

Is my understanding of that schematic change correct? I think that change makes PG_MODULE more correct, in that it won't try to boot the Zynq too early.

Thanks for any insight!

  • Sign in to reply
  • Cancel
  • ctammann
    0 ctammann over 10 years ago

    The carrier provides power to the I/O and transceiver rails, while not ideal to have the Zynq boot before all the rails are up, it can boot before these supplies are fully active.

    In the case of MicroZed without a carrier, the I/O banks are completely unpowered but you are still able to boot and work with the Zynq device.  Going forward the method used on the V2, which issues the reset release after all supplies are up, will be what is used.  If you have more questions please let me know.

    Thanks

    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer