Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Python-1300 on SVDK (PicoZed Carrier Card)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 357 subscribers
  • Views 1030 views
  • Users 0 members are here
Related

Python-1300 on SVDK (PicoZed Carrier Card)

e14 Contributor
e14 Contributor over 10 years ago

I was able to successfully capture video data utilizing the shipped video board (Aptina AR0134 1.2MP Camera Module) using Sphinx GEV Viewer.

To take it a step further I'd like to replace the Aptina AR0134 with a pin compatible module, the ON Semi PYTHON-1300.  After checking pinout compatibility I plugged in the camera module.  The documentation for the module states it's both MicroZed Embedded Vision Carrier Card and Smart Vison compatible (although indications are it's primarily a MicroZed EVCC module)

However, when I attempt to capture video from it using the same configuration as the Aptina AR0134 no video is captured.  Within the Sphinx tool when toggling on "Grab" an error message states "[ERROR] - GEVGetImage() [STATUS_TIMEOUT]"

Strangely the Width and Height default = 1.  I've manually changed them without resolution.

The console window displays the following:
[INFO] - Open stream channel.
[INFO] - Stream channel IP: 169.254.126.27
[INFO] - Stream channel port: 50164
[INFO] - Log mode: Detailed Log Info off
[INFO] - Log mode: Detailed Log Warning off
[INFO] - Log mode: Detailed Log Error off
[INFO] - Display corrupt frames: Yes
[INFO] - Allocate ring buffer for images.
[INFO] - Allocate index buffer for images.
[INFO] - Width: 1
[INFO] - Height: 1
[INFO] - PixelFormat: 0x01080001
[INFO] - PayloadSize: 64
[INFO] - PacketSize: 1364
[INFO] - PacketDelay: 500
[INFO] - Message Channel Device 2 -> stream channel start of transfer
[INFO] - Start acquisition time: 06:20:21
[INFO] - Message Channel Device 2 -> stream channel end of transfer
[INFO] - Free index buffer for images.
[INFO] - Free ring buffer for images.
[INFO] - Frames: 0, Errors: 0 Lost: 0.00 %
[INFO] - Packets: 0, Errors: 0 Lost: 0.00 %
[INFO] - 0.0 fps
[INFO] - Stop acquisition time: 06:20:22
[ERROR] - GEVGetImage() [STATUS_TIMEOUT]

As a comparison, this is what a successful transfer looks like in the console using the AR1034 (and, yes, there seems to be packet/drop issues in the "working" format:

INFO] - Open stream channel.
[INFO] - Stream channel IP: 169.254.126.27
[INFO] - Stream channel port: 58348
[INFO] - Log mode: Detailed Log Info off
[INFO] - Log mode: Detailed Log Warning off
[INFO] - Log mode: Detailed Log Error off
[INFO] - Display corrupt frames: Yes
[INFO] - Allocate ring buffer for images.
[INFO] - Allocate index buffer for images.
[INFO] - Width: 1280
[INFO] - Height: 960
[INFO] - PixelFormat: 0x01080001
[INFO] - PayloadSize: 1228800
[INFO] - PacketSize: 1364
[INFO] - PacketDelay: 500
[INFO] - Message Channel Device 2 -> stream channel start of transfer
[INFO] - Start acquisition time: 06:15:40
[ERROR] - ReadRegister[0x00000A00] Status: C008
[WARNING] - CCP lost.
[INFO] - CCP reconnection.
[INFO] - Free index buffer for images.
[INFO] - Free ring buffer for images.
[INFO] - Frames: 613, Errors: 0 Lost: 0.00 %
[INFO] - Packets: 552313, Errors: 305992 Lost: 55.40 %
[INFO] - 50.0 fps
[INFO] - Stop acquisition time: 06:15:52

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I recently purchased a picozed based smart vision development system from Sensor to Image via Avnet. It did not exactly jump to life out of the box, and no UART output was forethcoming, but after twenty minutes of screwing around I was able to get the Sphinx viewer to take a picture. Ten minutes later a message appeared indicating my 30 minute trial period had expired! Excuse me?

    Subsequently, I've examined the code and find that yes indeed there is a bit set by Sphinx that keeps the hardware from streaming after the "trial" period has expired.

    Can anyone clue me in to what is going on here? I am hoping I'm just being stupid and have overlooked something I was supposed to do (like registering, which I did).  Anybody?

    Or shall I just return this piece of BS to Avnet?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I recently purchased a picozed based smart vision development system from Sensor to Image via Avnet. It did not exactly jump to life out of the box, and no UART output was forethcoming, but after twenty minutes of screwing around I was able to get the Sphinx viewer to take a picture. Ten minutes later a message appeared indicating my 30 minute trial period had expired! Excuse me?

    Subsequently, I've examined the code and find that yes indeed there is a bit set by Sphinx that keeps the hardware from streaming after the "trial" period has expired.

    Can anyone clue me in to what is going on here? I am hoping I'm just being stupid and have overlooked something I was supposed to do (like registering, which I did).  Anybody?

    Or shall I just return this piece of BS to Avnet?