Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Python-1300 on SVDK (PicoZed Carrier Card)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 357 subscribers
  • Views 1030 views
  • Users 0 members are here
Related

Python-1300 on SVDK (PicoZed Carrier Card)

e14 Contributor
e14 Contributor over 10 years ago

I was able to successfully capture video data utilizing the shipped video board (Aptina AR0134 1.2MP Camera Module) using Sphinx GEV Viewer.

To take it a step further I'd like to replace the Aptina AR0134 with a pin compatible module, the ON Semi PYTHON-1300.  After checking pinout compatibility I plugged in the camera module.  The documentation for the module states it's both MicroZed Embedded Vision Carrier Card and Smart Vison compatible (although indications are it's primarily a MicroZed EVCC module)

However, when I attempt to capture video from it using the same configuration as the Aptina AR0134 no video is captured.  Within the Sphinx tool when toggling on "Grab" an error message states "[ERROR] - GEVGetImage() [STATUS_TIMEOUT]"

Strangely the Width and Height default = 1.  I've manually changed them without resolution.

The console window displays the following:
[INFO] - Open stream channel.
[INFO] - Stream channel IP: 169.254.126.27
[INFO] - Stream channel port: 50164
[INFO] - Log mode: Detailed Log Info off
[INFO] - Log mode: Detailed Log Warning off
[INFO] - Log mode: Detailed Log Error off
[INFO] - Display corrupt frames: Yes
[INFO] - Allocate ring buffer for images.
[INFO] - Allocate index buffer for images.
[INFO] - Width: 1
[INFO] - Height: 1
[INFO] - PixelFormat: 0x01080001
[INFO] - PayloadSize: 64
[INFO] - PacketSize: 1364
[INFO] - PacketDelay: 500
[INFO] - Message Channel Device 2 -> stream channel start of transfer
[INFO] - Start acquisition time: 06:20:21
[INFO] - Message Channel Device 2 -> stream channel end of transfer
[INFO] - Free index buffer for images.
[INFO] - Free ring buffer for images.
[INFO] - Frames: 0, Errors: 0 Lost: 0.00 %
[INFO] - Packets: 0, Errors: 0 Lost: 0.00 %
[INFO] - 0.0 fps
[INFO] - Stop acquisition time: 06:20:22
[ERROR] - GEVGetImage() [STATUS_TIMEOUT]

As a comparison, this is what a successful transfer looks like in the console using the AR1034 (and, yes, there seems to be packet/drop issues in the "working" format:

INFO] - Open stream channel.
[INFO] - Stream channel IP: 169.254.126.27
[INFO] - Stream channel port: 58348
[INFO] - Log mode: Detailed Log Info off
[INFO] - Log mode: Detailed Log Warning off
[INFO] - Log mode: Detailed Log Error off
[INFO] - Display corrupt frames: Yes
[INFO] - Allocate ring buffer for images.
[INFO] - Allocate index buffer for images.
[INFO] - Width: 1280
[INFO] - Height: 960
[INFO] - PixelFormat: 0x01080001
[INFO] - PayloadSize: 1228800
[INFO] - PacketSize: 1364
[INFO] - PacketDelay: 500
[INFO] - Message Channel Device 2 -> stream channel start of transfer
[INFO] - Start acquisition time: 06:15:40
[ERROR] - ReadRegister[0x00000A00] Status: C008
[WARNING] - CCP lost.
[INFO] - CCP reconnection.
[INFO] - Free index buffer for images.
[INFO] - Free ring buffer for images.
[INFO] - Frames: 613, Errors: 0 Lost: 0.00 %
[INFO] - Packets: 552313, Errors: 305992 Lost: 55.40 %
[INFO] - 50.0 fps
[INFO] - Stop acquisition time: 06:15:52

  • Sign in to reply
  • Cancel
Parents
  • albertabeef
    0 albertabeef over 10 years ago

    The reference designs for the SVDK are created by Sensor To Image, a german company specializing in machine vision connectivity.

    Sensor To Image provides IP cores.  They also provide reference designs to allow customers to evaluate their cores before purchasing the IP cores.  The "30 minute timebomb" is occuring in the IP core inside the hardware design.  This is a very common practise from third party IP providers.

    Please note that the price of the SVDK does not include the price of the Sensor To Image IP cores.  If you want to purchase the Sensor To Image IP cores, please contact Sensor To Image.

    Regards,

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • albertabeef
    0 albertabeef over 10 years ago

    The reference designs for the SVDK are created by Sensor To Image, a german company specializing in machine vision connectivity.

    Sensor To Image provides IP cores.  They also provide reference designs to allow customers to evaluate their cores before purchasing the IP cores.  The "30 minute timebomb" is occuring in the IP core inside the hardware design.  This is a very common practise from third party IP providers.

    Please note that the price of the SVDK does not include the price of the Sensor To Image IP cores.  If you want to purchase the Sensor To Image IP cores, please contact Sensor To Image.

    Regards,

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to albertabeef

    Perhaps you should clearly state in your marketing literature that without purchasing additional licenses, this board will become useless after 30 minutes.

    Shall I call my Avnet rep and see if he was aware of this?