Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Zynq 7015/7030
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 357 subscribers
  • Views 299 views
  • Users 0 members are here
Related

Zynq 7015/7030

e14 Contributor
e14 Contributor over 10 years ago

hi,

ist zynq 16 und 30 pin compatible? How can i realise an error signal on the picozed? oder at which pin could connect the LED to signalized error because i alreadx have on(FPGA_DONE) for successful booting of the FPGA.

Could i also use the JX(1,2)_SE like normal I/O pins?

thanks for the help

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

    Yes, the PicoZed 7015 and PicoZed 7030 are pin compatible. Keep in mind that Bank 34 and Bank 35 IO Voltage MUST be 1.8V only when using a PicoZed 7030 to avoid damaging the Zynq 7030 device. Take a look at the PicoZed 7015/7030 Users Guide for more details:

    http://zedboard.org/support/documentation/4736

    Yes the JS '-SE' signals are normal 'single-ended' I/O pins.

    You will need to be more clear about your error signal and LED question, I am not sure what you are asking.

    -Gary