Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design VBUS ans USB OTG
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 356 subscribers
  • Views 273 views
  • Users 0 members are here
Related

VBUS ans USB OTG

e14 Contributor
e14 Contributor over 11 years ago

Hi,
I'm currently designing a carrier board for the picozed. I want to configure the USB as an OTG device. I did review the phy datasheet and the schematics. I observed that USB_VBUS_OTG has a lot of capacitor both on the picozed itself (C3) and on the carrier board (C167).

In normal USB OTG mode these capacitor are connected trough a 1k resistor to the USB_VBUS.

Are the 100uF capacitor needed? I'm not sure of the effect with OTG where this should be quite lower?

Maybe I'm just missing something and the USB_VBUS_OTG is used as a power rail somewhere?

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 11 years ago

    According to the USB3320 datasheet, to use it in OTG mode:

    •   Rvbus = 1k-ohm (Table 5.7)
    •   The system is required to source 5V on VBUS (5.6.3)
    •   Cvbus between 1uF and 6.5uF (Table 8.2) -- you do NOT want the 100 uF

    Bryan