Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design SATA for PicoZed?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 357 subscribers
  • Views 681 views
  • Users 0 members are here
Related

SATA for PicoZed?

e14 Contributor
e14 Contributor over 11 years ago

Greetings,

I'm looking at the PicoZed as a controller for a data acquisition system (size constraints preclude the mini-ITX).  The only thing missing is a SATA connection, so I'm wondering if there is any reason a 7015- or 7030-based picozed could not work with the MLE SATA core?  I understand I'll have to provide power and a clock and also connect to the SATA connector through the headers,  that's OK.

Has anyone done this, or with a different SATA IP core?

Looks like the MMP could be an option too, but a significantly more expensive one.

TIA,
  Fred

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The PicoZed should work with SATA but we do not have any plans currently to create any add-on hardware or a reference design.

     

    The MMP will support SATA with the MMP BaseBoard II along with the Xilinx XM104 FMC or via a custom baseboard with a SATA connector.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Thanks Gary.  We will need a custom baseboard anyway to break out connectors for D/A and A/D boards, so adding the SATA connector, clock, and power is OK.  The MPP Baseboard is too big for our application and does not remove the need for the connector board, so it doesn't really help except to use as a reference design.  I was just looking for some confidence that the MLE core would work with the 7015 or 7030 since the PL is from a different device family (Artix vs. Kintex).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The Zynq 7030 PL is Kintex fabric, so it might be a safer choice.

     

    -Gary