Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Is it possible to add a usb hub chip on the custom carrier for picozed?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 357 subscribers
  • Views 461 views
  • Users 0 members are here
Related

Is it possible to add a usb hub chip on the custom carrier for picozed?

e14 Contributor
e14 Contributor over 9 years ago

I have recently added a usb hub chip (CY7C65634-48AXC) in a custom carrier board for picozed 7015 to support 2 USB host ports, but FAILED.   

BOOT LOG:

usb 1-1.1: device descriptor read/64, error -32
usb 1-1.1: new full-speed USB device number 5 using ci_hdrc
usb 1-1.1: device not accepting address 5, error -32
usb 1-1.1: new full-speed USB device number 6 using ci_hdrc
 
LSUSB:
  root@pz-7015-2016-2:~# lsusb
  Bus 001 Device 002: ID 04b4:6570 Cypress Semiconductor Corp.
  Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
   
 

I noticed that the Mini-ITX board has used the combination of USB3320 + CY7C65632-28QFN, but the REFCLK input of USB3320 is a 12 MHz clock which is different from a 24 MHz clock input in Picozed7015. 

 

I suspect that the problem I encountered comes from the clock frequency.  Question is, is it possible to add a usb hub chip on the custom carrier for picozed?

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Wuhingbang,

    Yes it is possible to add a usb hub chip to a customer carrier card for PicoZed. As you have experienced, you need a 24MHz input clock to interface with the PicoZeds USB 2.0. You are free to put a different  clock on your circuit to make it compatible with your design, as you pointed out the Mini-ITX has a circuit you can mimic. If you choose this path it is at your own risk. We provided a working example for the MIni_itx It will be your responsibility for properly porting it over for the PicoZed Som.

    --Josh