Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Can't boot from eMMC in Standard Speed Mode at -30degC
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Subscribers 359 subscribers
  • Views 3554 views
  • Users 0 members are here
Related

Can't boot from eMMC in Standard Speed Mode at -30degC

e14 Contributor
e14 Contributor over 7 years ago

At -15degC its ok but it needs to boot at -30degC.

I have at least 2 rev C Picozed 7030's with this problem and have complied with the advisory note by operating in standard speed mode at 25MHz (section 3.7 in the Avnet Errata).  Signal eMMC_CLK has been measured at 25MHz to verify this.

Do I have faulty boards, or is there anything else I've overlooked ?

I can provide screen dumps from the serial port or other information as required.

Please advise.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 7 years ago

    Hi Bryan,

    Thanks for the reply. We aren’t using PetaLinux, we’re using bitbake and the meta-xilinx Yocto recipe layers to build Linux and U-Boot. Please could you point us to the source code and/or configuration files that apply these settings to U-Boot and Linux (patches will do).

    Regards,

    Robert

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 7 years ago

    Hi Bryan,

    Thanks for the reply. We aren’t using PetaLinux, we’re using bitbake and the meta-xilinx Yocto recipe layers to build Linux and U-Boot. Please could you point us to the source code and/or configuration files that apply these settings to U-Boot and Linux (patches will do).

    Regards,

    Robert