Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design zedboard and picozed booting
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 708 views
  • Users 0 members are here
Related

zedboard and picozed booting

e14 Contributor
e14 Contributor over 10 years ago

Hello,

I want to know ,can picozed booting with QSPI like zedboard ?

For example,connect arm hw

                  source ps7_init.tcl

                 .........

 

                

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 10 years ago

    Hello Wangy,

    Yes your PicoZed can boot by QSPI. If you refer to our Zynq Software Labs : 

    http://zedboard.org/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20133-201441-20152-and-20162

    specifically lab 7, it goes into how to create a .mcs file that is used to program the qspi.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jafoste4

    Hello JFoster, I refered to lab7 to program flash ,but failed,

    console shows:

                                       ****** Xilinx Program Flash

    ****** Program Flash v2015.4 (64-bit)
      **** SW Build 1412921 on Wed Nov 18 09:43:45 MST 2015
        ** Copyright 1986-2015 Xilinx, Inc. All Rights Reserved.
     
    Connecting to hw_server @ TCP:127.0.0.1:3121
     
    Connected to hw_server @ TCP:127.0.0.1:3121
    Available targets and devices:
    Target 0 : jsn-DLC10-000014d2f51c01
    Device 0: jsn-DLC10-000014d2f51c01-4ba00477-0
    Target 1 : jsn1
     
    ERROR: Failed to open Target Cable Node 59866048 on TCP:127.0.0.1:3121
     
    How do I solve?
    Thanks,
    wangy,
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jafoste4

    Hello JFoster, I refered to lab7 to program flash ,but failed,

    console shows:

                                       ****** Xilinx Program Flash

    ****** Program Flash v2015.4 (64-bit)
      **** SW Build 1412921 on Wed Nov 18 09:43:45 MST 2015
        ** Copyright 1986-2015 Xilinx, Inc. All Rights Reserved.
     
    Connecting to hw_server @ TCP:127.0.0.1:3121
     
    Connected to hw_server @ TCP:127.0.0.1:3121
    Available targets and devices:
    Target 0 : jsn-DLC10-000014d2f51c01
    Device 0: jsn-DLC10-000014d2f51c01-4ba00477-0
    Target 1 : jsn1
     
    ERROR: Failed to open Target Cable Node 59866048 on TCP:127.0.0.1:3121
     
    How do I solve?
    Thanks,
    wangy,