Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Clock SMA Connector
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 356 subscribers
  • Views 405 views
  • Users 0 members are here
Related

Clock SMA Connector

marcomercuri85
marcomercuri85 over 9 years ago

Dear all,

 

I'm using the 7030 PicoZed + FMC Carrier Card V2.

 

Is it possible to take out a clock from the SMA connector?

 

I tried to connect FCLK_CLK0 or a clock generate with Clocking Wizard to TX1_P or TX1_P but I get errors while generating the bitsteam.

 

These are my constraints:

set_property PACKAGE_PIN W4 [get_ports clk_out1];
set_property IOSTANDARD LVCMOS33 [get_ports clk_out1];

 

Thanks a lot.

 

Best Regards,

Marco

  • Sign in to reply
  • Cancel
  • drozwood90
    0 drozwood90 over 9 years ago

    Hi there,

    If you check the schematic, you will see that the circuit implemented does not allow for this.  The best option I can offer is to use the IDT Femtoclock and mirror your input clock from that part to both the debug test points as well as the MGT input pins. 

    The transceiver pins can only transmit from the transceiver circuitry.  They are not general purpose pins as almost all of the rest of the IO.

    --Dan