Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Using external reference TCXO on PicoZed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 358 subscribers
  • Views 749 views
  • Users 0 members are here
  • external clock
Related

Using external reference TCXO on PicoZed

400garrison
400garrison over 6 years ago

I have a question regarding the PicoZED 7030 SOM.  We are considering using it in an upcoming baseband module, and I was wondering if you could help me with a question regarding the onboard clock oscillator. On our current (existing) baseband module, we use a VT-803 TCXO for the 52MHz reference.  This part (VT-803) has an overall stability (including aging) of less than 10ppm.  The PicoZED uses a Abracon ASDMB MEMS oscillator that has at best 10ppm of stability (with an additional 5ppm for aging).

 

Is there a different part that could be used in place of this MEMS oscillator, or can we feed in our own clock reference to the PicoZED?

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 6 years ago +1 suggested
    400garrison Looking at Changing the 33.33333MHz Oscillator | Zedboard , seems like it can be done if the pins are compatible and the clock is adjusted for the higher frequency so the UART will work.
  • clem57
    0 clem57 over 6 years ago

    400garrison Looking at Changing the 33.33333MHz Oscillator | Zedboard , seems like it can be done if the pins are compatible and the clock is adjusted for the higher frequency so the UART will work.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • 400garrison
    0 400garrison over 6 years ago in reply to clem57

    So no way to plug in an external clock source?