Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design eMMC init at Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 356 subscribers
  • Views 763 views
  • Users 0 members are here
  • emmc
  • linux
Related

eMMC init at Linux

itzikhaim
itzikhaim over 6 years ago

We have a problem when trying to enable the eMMC (soldered-chip)  at picozed (zynq zc702) evalutation board at Linux.

The board is rev. E.

We are using an HDF file from our firmware engineer which enabled the ps7_sd_0 and ps7_sd_1 entities. The good thing is that we can fully use the eMMC at u-boot (using mmc tool) -built from Xilinx repo (u-boot-xlnx-2019.01).

We are building linux kernel 4.19.0 from Xilinx repository and tried various device trees (the deafult disable the eMMC chip)- but non of them are working.

We get the following error when booting linux:

mmc1: Got command interrupt 0x00030000 even though no command operation was in progress.
sdhci: =========== SDHCI REGISTER DUMP ===========
sdhci: Sys addr: 0x00000000 | Version:  0x00008901
sdhci: Blk size: 0x00000000 | Blk cnt:  0x00000000
sdhci: Argument: 0x00000000 | Trn mode: 0x00000000
sdhci: Present:  0x00ef0000 | Host ctl: 0x00000001
sdhci: Power:    0x0000000f | Blk gap:  0x00000000
sdhci: Wake-up:  0x00000000 | Clock:    0x00004007
sdhci: Timeout:  0x00000000 | Int stat: 0x00000000
sdhci: Int enab: 0x00ff0003 | Sig enab: 0x00ff0003
sdhci: AC12 err: 0x00000000 | Slot int: 0x00000000
sdhci: Caps:     0x69ec0080 | Caps_1:   0x00000000
sdhci: Cmd:      0x0000371a | Max curr: 0x00000001
sdhci: Host ctl2: 0x00000000
sdhci: ADMA Err: 0x00000000 | ADMA Ptr: 0x00000000
sdhci: ===========================================

 

We tried the following previously supported answers:

https://forums.xilinx.com/t5/Processor-System-Design/Zynq-SDIO-via-EMIO/td-p/327479

https://forums.xilinx.com/t5/Embedded-Linux/Problems-with-using-a-second-SDIO-controller/td-p/442766

Note that we are not using the SDIO via EMIO (only directly from PS pins/mux).

Also, tried to add into the device-tree the "wp-inverted;" property as suggested at this forum:

SDcard not writeable on PicoZed Rev E board (Rev C board works) ?

 

But still no progress - please your help.