Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Reading back configuration memory
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 356 subscribers
  • Views 2725 views
  • Users 0 members are here
Related

Reading back configuration memory

jfioriglio
jfioriglio over 4 years ago

For the PICOZED board, how do I read configuration Memory? Need to read out configuration memory on field failures.

  • Sign in to reply
  • Cancel

Top Replies

  • bhfletcher
    bhfletcher over 4 years ago +1 verified
    Are you talking about the QSPI? You can use the Hardware Manager and a JTAG connection to readback QSPI or do a verify. Bryan
  • bhfletcher
    +1 bhfletcher over 4 years ago

    Are you talking about the QSPI? You can use the Hardware Manager and a JTAG connection to readback QSPI or do a verify.

    Bryan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • jfioriglio
    0 jfioriglio over 4 years ago in reply to bhfletcher

    Yes,  I am trying a read data back from QSPI.  I open Hardware Manager, Autoconnect and then type in the following at TCL prompt:

    readback_hw_cfgmem -file test.bin -hw_cfgmem \ [get_property PROGRAM.HW_CFGMEM [lindex [get_hw_devices] 0]].

    I get an error saying -hw_cfgmem option is not valid.  

    What am I doing wrong?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 4 years ago in reply to jfioriglio

    I apologize for giving you bad information previously. Zynq devices do not support QSPI readback with Hardware Manager. The best advice that I could find was on the Xilinx forums here:

    https://support.xilinx.com/s/question/0D52E00006hpPtwSAE/zynq-7000-read-qspi-flash-to-file?language=en_US

    Unfortunately, no specific U-boot commands were shared, so I did a little experimenting with a MicroZed that I have here. I loaded up the Linux pre-built image onto an SD Card from the Avnet BSP, then booted from SD Card, making sure to interrupt at the U-boot stage. After that, then the commands that I followed were:

    • sf probe 0 0 0
    • sf read 0x08000000 0 0x1000000
    • fatwrite mmc 0 0x08000000 boot_qspi.bin 0x1000000
    • fatls mmc 0

     

    Where

    • 0x08000000 is a location in DDR to temporarily store stuff
    • 0 is the offset in the QSPI
    • 0x1000000 is 16MB length
    • mmc is the SD Card interface
    • boot_qspi.bin is the filename on the SD Card

    Bryan