Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio LO leakage as a function of TX power
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 358 subscribers
  • Views 705 views
  • Users 0 members are here
Related

LO leakage as a function of TX power

e14 Contributor
e14 Contributor over 9 years ago

Hi, I plan to use PicoZED SDR as a simple signal generator. I wonder how the LO leakage behaves as a function of transmitted signal power? For example, what can be seen at the transmitter output connector at LO frequency when the baseband signal is totally off? The frequency would be around 1.4GHz.

- Ivalo

  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 9 years ago

    "how the LO leakage behaves as a function of transmitted signal power?"

     

    The analog devices EngineerZone is the place to ask questions about AD9361 performance.

     

    Thanks,

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to mbrown

    AD9361 performance may be the largest contributor to leakage, however part of the leakage is caused by parasitics which depend on the board design, I think. So I would be happy if someone would plug a spectrum analyzer to the TX connector, set the signal amplitude to zero and see how much power is transmitted on the LO frequency :)
    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to mbrown

    AD9361 performance may be the largest contributor to leakage, however part of the leakage is caused by parasitics which depend on the board design, I think. So I would be happy if someone would plug a spectrum analyzer to the TX connector, set the signal amplitude to zero and see how much power is transmitted on the LO frequency :)
    Thanks!