Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio Pricing and Availability of PicoZed SDR RF Module with PA, LNA, and TDD switch
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 358 subscribers
  • Views 1356 views
  • Users 0 members are here
Related

Pricing and Availability of PicoZed SDR RF Module with PA, LNA, and TDD switch

e14 Contributor
e14 Contributor over 10 years ago

Matt,
Do you have pricing and availability for the Avnet AES-PZSDR-RFMOD-TDD-G?

Thanks,
Craig

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Please note the change to part number: AD-PZSDR2400TDD-EB

    2.4GHz TDD RF Personality Module for the Avnet PicoZed SDR

    The AD-PZSDR2400TDD-EB module connects onto the Avnet PicoZed SDR FMC Carrier Card (AES-PZSDRCC-FMC-G) http://picozed.org/product/picozed-sdr-som-development-kit

    AD-PZSDR2400TDD-EB provides a tunable path to condition the transmit or receive RF signals of the AD9361. Selection of TX or RX path is achieved by the 200MHz to 2.7GHz SPDT switch HMC546LP2 controlled by the FPGA and accompanying software.
    The transmit path consists of a 2.4GHz filter, half watt driver amplifier ADL5324 and 2 watt power amplifier HMC921. The receive path consists of the same 2.4GHz filter as well as a low loss LNA HMC669.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Please note the change to part number: AD-PZSDR2400TDD-EB

    2.4GHz TDD RF Personality Module for the Avnet PicoZed SDR

    The AD-PZSDR2400TDD-EB module connects onto the Avnet PicoZed SDR FMC Carrier Card (AES-PZSDRCC-FMC-G) http://picozed.org/product/picozed-sdr-som-development-kit

    AD-PZSDR2400TDD-EB provides a tunable path to condition the transmit or receive RF signals of the AD9361. Selection of TX or RX path is achieved by the 200MHz to 2.7GHz SPDT switch HMC546LP2 controlled by the FPGA and accompanying software.
    The transmit path consists of a 2.4GHz filter, half watt driver amplifier ADL5324 and 2 watt power amplifier HMC921. The receive path consists of the same 2.4GHz filter as well as a low loss LNA HMC669.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mbrown
    0 mbrown over 10 years ago in reply to e14 Contributor

    The module is open for orders on the Analog Devices product page:

     

    http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/ad-pzsdr2400tdd-eb.html

     

    Thanks,
    Matt