Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio VCCINT-0P95V Below Spec
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 911 views
  • Users 0 members are here
Related

VCCINT-0P95V Below Spec

e14 Contributor
e14 Contributor over 10 years ago

On multiple PicoZed SDR's we are observing VCCINT-0P95V at 0.919V, which is below min spec (0.93V).  I traced the problem to excessive voltage drop across inductor E6.  (VOUT3 is at 0.964V).

 

Just an observation so far, we seem to be operating fine despite the low rail.

 

I would use the ADM1166 margining feature to boost the rail, but I am worried about over-voltaging VCC-BRAM, which is also fed from VOUT3.  VCC-BRAM is only exposed on the bottom of the SOM (E5 and C194) in the middle of the connectors, so is a difficult rail to probe.

 

-Jer

  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 10 years ago

    The DC resistance of E6 is, as you've both identified (thank you!), turned out to be a problem for this narrow tolerance Zynq rail.

    In fact our designers recognized a need for higher current capacity for the 0.95V rail and we are in the middle of building prototypes of a Rev D module that removes that ferrite component and increases the capacity to around 6A. The reduced filtering is not expected to have any negative effects on the overall system.

    Shorting E6 is the easiest remedy for now. It's a big component and easily found (see below).

    image

     

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • mbrown
    0 mbrown over 10 years ago

    The DC resistance of E6 is, as you've both identified (thank you!), turned out to be a problem for this narrow tolerance Zynq rail.

    In fact our designers recognized a need for higher current capacity for the 0.95V rail and we are in the middle of building prototypes of a Rev D module that removes that ferrite component and increases the capacity to around 6A. The reduced filtering is not expected to have any negative effects on the overall system.

    Shorting E6 is the easiest remedy for now. It's a big component and easily found (see below).

    image

     

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to mbrown

    Matt, shorting out E6 solved this problem for us. The VCCINT voltage is now in spec at 0..944V and the board passes all tests without E6.

    Thanks for your help!