Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio Frequency band
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 358 subscribers
  • Views 612 views
  • Users 0 members are here
Related

Frequency band

e14 Contributor
e14 Contributor over 10 years ago

I have a couple of questions from the customer.

1. The customer is using PicoZed SDR Z7035/AD9361 SOM
  (AES-Z7PZ-SDR2-G). He wants to use it for 5.7GHz.
   Although the results which he gets in 2.4GHs is
   the same as the datasheet, he cannot get
   the same results as the datasheet in 5.7GHz.
   He wonders if PicoZed SDR he has gotten is
   adjusted for 2.4GHz.
   Are there PicoZed SDR tuned to be in the
   indivisual band, 800MHz, 2.4GHz, 5.5GHz and so on ?
   If there is PicoZed SDR for 5.5GHz, can we get it ?

2. Is it possible that he tunes PicoZed SDR to be for
   5.7GHz with using software setting ?

The results he gets are following.
In the case of 2.4GHz signal output, an image is found under -60dBc of the desired signal.
But in the case of 5.7GHz signal output, an image is found under -40dBc of the desired signal.
The datasheet says that the carrier leakage is -50dBc in both 2.4GHs and 5.5GHz.
The customer is in trouble.

Best Regards.

  • Sign in to reply
  • Cancel
Parents
  • rgetz
    0 rgetz over 10 years ago

    That has not been our results from our tests on the PicoZed Z7035/AD9361 either.

    The output/balun stage on the AD9361 is identical to that of the FMCOMMS3, and there is some known droop in some specs at very low, and very high - the EVM number doesn't change that much (which would be impacted alot by images).

    https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms3-ebz/hardware/card_specification

    -Robin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • rgetz
    0 rgetz over 10 years ago

    That has not been our results from our tests on the PicoZed Z7035/AD9361 either.

    The output/balun stage on the AD9361 is identical to that of the FMCOMMS3, and there is some known droop in some specs at very low, and very high - the EVM number doesn't change that much (which would be impacted alot by images).

    https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms3-ebz/hardware/card_specification

    -Robin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer