Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio Can't drop sample rate below ~2.1MSPS
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 359 subscribers
  • Views 908 views
  • Users 0 members are here
Related

Can't drop sample rate below ~2.1MSPS

e14 Contributor
e14 Contributor over 10 years ago

I'm running against a processing speed issue with the PicoZed SDR that would likely work better with a lower sampling rate. I'm unable to set the sample rate below about 2.1 MSPS right now, though. The actual minimum seems to be somewhere between 2.083 and 2.084 MSPS. The examples in the GRC files that come with the Analog SD card start at ~1.5 MSPS, which doesn't work at all. Do I need to set another clock somewhere to get lower sample rates? If so, how do I do that?

Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • andrew_senior
    andrew_senior over 9 years ago +1 verified
    Not sure if you're still looking for an answer to this 5 months on, but just in case, the reason you can't go below 2.084 Msps is two fold: 1. The minimum ADC rate is 25 MHz, according to this post from…
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Thanks for the reply. I'm actually not able to use 1.536. Anything lower than ~2.084 gives me "Unable to write attribute in_voltage_sampling_frequency: -22" and the same for "out_voltage_sampling_frequency". This is using the "FMComms2/3/4 Source" and "...Sink" blocks inside GRC.

    When I run the ADI IIO Oscilloscope tool, I also am unable to go below ~2.084 MSPS. Any setting below that causes the value to reload and return to its previous value.

    Possibly related is that I can't set the manual Rx gain to anything except 71.0. I also can't set the Tx attenuation in the GRC Sink ... I just get "Unable to write attribute out_voltage0_hardwaregain: -22" and the same for "out_voltage1_hardwaregain".

    The ADI IIO tool is interesting and seems to offer a ton of control over the hardware. Is there a good reference that can help me understand what its controls do?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Thanks for the reply. I'm actually not able to use 1.536. Anything lower than ~2.084 gives me "Unable to write attribute in_voltage_sampling_frequency: -22" and the same for "out_voltage_sampling_frequency". This is using the "FMComms2/3/4 Source" and "...Sink" blocks inside GRC.

    When I run the ADI IIO Oscilloscope tool, I also am unable to go below ~2.084 MSPS. Any setting below that causes the value to reload and return to its previous value.

    Possibly related is that I can't set the manual Rx gain to anything except 71.0. I also can't set the Tx attenuation in the GRC Sink ... I just get "Unable to write attribute out_voltage0_hardwaregain: -22" and the same for "out_voltage1_hardwaregain".

    The ADI IIO tool is interesting and seems to offer a ton of control over the hardware. Is there a good reference that can help me understand what its controls do?