Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio picozed can not establish TCP/IP connection with PC
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 358 subscribers
  • Views 448 views
  • Users 0 members are here
Related

picozed can not establish TCP/IP connection with PC

e14 Contributor
e14 Contributor over 10 years ago

I have connect my PC and picozed through RJ45 connector, and set my PC and picozed in the same subnet. And PC 's IP is 192.168.3.1, the board is 192.168.3.2, there mask is 255.255.255.0. after that, I run the "ping 192.168.3.2"command in the dos window of PC, it can get response, but when i want to tansmit data from PC to board, the error occurred. it told me ,the hardware have no response. and I havd installed the add-on  apps or plugs in the matlab. and the most important thing is my PC can not connect with the internet or router.wish you solution.thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago
    If you wish to perform radio-in-the-loop simulation from MATLAB/Simulink you must have installed Communications System Toolbox Support Package for Xilinx Zynq-Based Radio http://www.mathworks.com/help/supportpkg/xilinxzynqbasedradio/index.html
     
    This is fully explained in this video: http://microzed.org/videos/qpsk-receiver-radio-loop
     
    You can then configure and test communication between the host and PicoZed SDR from Guided Host-Radio Hardware Setup http://www.mathworks.com/help/supportpkg/xilinxzynqbasedradio/ug/guided-host-radio-hardware-setup.html?s_tid=gn_loc_drop
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago
    If you wish to perform radio-in-the-loop simulation from MATLAB/Simulink you must have installed Communications System Toolbox Support Package for Xilinx Zynq-Based Radio http://www.mathworks.com/help/supportpkg/xilinxzynqbasedradio/index.html
     
    This is fully explained in this video: http://microzed.org/videos/qpsk-receiver-radio-loop
     
    You can then configure and test communication between the host and PicoZed SDR from Guided Host-Radio Hardware Setup http://www.mathworks.com/help/supportpkg/xilinxzynqbasedradio/ug/guided-host-radio-hardware-setup.html?s_tid=gn_loc_drop
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer