Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio PicoZed SDR compatibility with ON PYTHON-1300-C Camera Module
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 359 subscribers
  • Views 1499 views
  • Users 0 members are here
Related

PicoZed SDR compatibility with ON PYTHON-1300-C Camera Module

jshimoun1
jshimoun1 over 9 years ago

I have a Picozed SDR 2x2 and SDR FMC Carrier Card included with the PicoZed SDR Development Kit. I would like to connect the ON Python 1300 Camera Module to the Picozed through the PCI port on the carrier card.

 

I currently have the standard image booted on the SD card and I would like to use the camera interface through Linux drivers instead of modifying the hardware image. Is this possible? Can I simply modify the device tree to include the Python Camera? Are there drivers that I can download for the camera?

  • Sign in to reply
  • Cancel
Parents
  • jshimoun1
    0 jshimoun1 over 9 years ago

    I was able to get the camera connected using a BOOT.bin file in one of the reference designs. Is there a way to use the camera within the Linux OS? Right now, my only option is to view the camera feed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • albertabeef
    0 albertabeef over 9 years ago in reply to jshimoun1

    Refer to one of the following design, created for the PicoZed Embedded Vision Kit.

       PZEMBV PYTHON-1300-C SDSoC platform, Vivado 2016.2

    This design will contain the following components that you can reuse to enable the PYTHON-1300-C camera on the PZSDR platform

       pzembv/boot/how-to-build-this-image.txt => instructions on how to build the petalinux binaries, with the linux kernel patch for the PYTHON-1300-C camera

       pzembv/boot/patch/mzembv-python-2016.2-v1.0.patch => linux kernel patch for the PYTHON-1300-C

       pzembv/boot/petalinux/subsystems/linux/configs/device-tree/pzembv-vcap-python1300.dtsi => device tree snippet for the PYTHON-1300-C capture pipeline

       pzembv/vivado/pzembv.xpr => Vivado/IPI project, containing the PYTHON-1300-C capture pipeline, corresponding to pzembv-vcap-python1300.dtsi

     

    Hope this helps !

    Regards,

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • albertabeef
    0 albertabeef over 9 years ago in reply to jshimoun1

    Refer to one of the following design, created for the PicoZed Embedded Vision Kit.

       PZEMBV PYTHON-1300-C SDSoC platform, Vivado 2016.2

    This design will contain the following components that you can reuse to enable the PYTHON-1300-C camera on the PZSDR platform

       pzembv/boot/how-to-build-this-image.txt => instructions on how to build the petalinux binaries, with the linux kernel patch for the PYTHON-1300-C camera

       pzembv/boot/patch/mzembv-python-2016.2-v1.0.patch => linux kernel patch for the PYTHON-1300-C

       pzembv/boot/petalinux/subsystems/linux/configs/device-tree/pzembv-vcap-python1300.dtsi => device tree snippet for the PYTHON-1300-C capture pipeline

       pzembv/vivado/pzembv.xpr => Vivado/IPI project, containing the PYTHON-1300-C capture pipeline, corresponding to pzembv-vcap-python1300.dtsi

     

    Hope this helps !

    Regards,

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jshimoun1
    0 jshimoun1 over 9 years ago in reply to albertabeef

    It looks like that tutorial is designed for the Z7030. While the kernel patch and design tree (and other components) also work with the Z7035 if I use the correct BSP?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jshimoun1
    0 jshimoun1 over 9 years ago in reply to jshimoun1

    *Will