Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio PicoZed SDR PL ETH problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 357 subscribers
  • Views 853 views
  • Users 0 members are here
Related

PicoZed SDR PL ETH problem

e14 Contributor
e14 Contributor over 9 years ago

Hi.

We have a PicoZed SDR paired with an Avnet eval board (AES-PZSDRCC-FMC-G). I'm having trouble with the 2nd ethernet interface (PL), which is connected to a Marvel 88E1512 PHY over RGMII on the carrier card. Going through PS (GEM1) is not an option because our design is PL based.

I'm on Vivado 2015.1, using TEMAC core v9.0. The problem is that I cannot seem to receive data properly on the TEMAC core. When I scope the TEMAC core, I see packets being converted properly from RGMII to GMII. But within the core, the data gets corrupted where half the bytes are dropped. I get a bad frame flag and nothing comes out the M_AXIS bus.

Here's a screenshot from the debug core (all the signals are within the TEMAC core):

http://picozed.org/sites/default/files/u118491/2.png

I've also probed the PHY with an oscope and the RXC looks good @ 125MHz. I'm also certain the 2nd ethernet interface is working properly because the pre-compiled SD card that came with the eval board boots up and I can bring it up with ifconfig on a UART terminal. But this is not ideal because we would like to go PL-only for the 2nd ethernet.

 

Thank you, in advance.

-- Benimage

  • Sign in to reply
  • Cancel
  • mbrown
    0 mbrown over 9 years ago

    Hi Ben,

    We don't have a PL-based Ethernet design for PicoZed SDR.  However, we've passed your request to the Avnet FAE in your area who will contact you with a possible solution.

     

    Thanks,

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer