Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio PicoZed SDR Z7035-AD9361 Power Sequencer Update
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 359 subscribers
  • Views 1339 views
  • Users 0 members are here
Related

PicoZed SDR Z7035-AD9361 Power Sequencer Update

mbrown
mbrown over 10 years ago

The document linked below explains PicoZed SDR 2x2 System-on-Module (SOM) power up issues that have been occasionally reported. This pertains only to part number AES-Z7PZ-SDR2-G. This document also provides the steps necessary to update the firmware of the power sequencer located on the SOM, which resolves the power up issues. This critical update should be applied to all PicoZed 2x2 SOMs to ensure reliable operation.

 

https://avnet.egnyte.com/dl/9PD26RxEwJ/PicoZed_SDR_Z7035-AD9361_Power_Sequencer_Update_v1.4.pdf_

 

The SOM User Guide has been updated accordingly.

 

/Matt

  • Sign in to reply
  • Cancel
Parents
  • iampkim
    0 iampkim over 9 years ago

    I have a custom carrier using 5V for JX_VIN and 3.3V for VCCO_12 and VCCO_13.  I'm not using the MGT bank so have connected MGTAVCC and MGTAVTT to gnd.  Following the procedure outlined in the pdf, I still see pulsing D3 and VIN_EN from ADM1166 never enables VIN.

    Are there other HW configurations on my custom carrier that could be missing?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • iampkim
    0 iampkim over 9 years ago

    I have a custom carrier using 5V for JX_VIN and 3.3V for VCCO_12 and VCCO_13.  I'm not using the MGT bank so have connected MGTAVCC and MGTAVTT to gnd.  Following the procedure outlined in the pdf, I still see pulsing D3 and VIN_EN from ADM1166 never enables VIN.

    Are there other HW configurations on my custom carrier that could be missing?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mbrown
    0 mbrown over 9 years ago in reply to iampkim

    What you described should work just fine. Let's confirm a few things.

    1. You successfully updated the ADM1166 firmware by attaching the SDR2x2 SOM to an Avnet carrier and following the PDF instructions?

    2. Did it power up on the Avnet carrier after reprogramming the ADM1166?

    3. Can you measure the 5.0V, and 3.3V rails on your carrier and confirm they are within spec (Table 1 in the PDF)?

    4. Are you running the out-of-box SD card image on the SOM, or something custom?

    5. Which revision of SOM do you have RevC or Rev E?

     

    Let's start there. We should be able to diagnose this quickly.

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iampkim
    0 iampkim over 9 years ago in reply to mbrown

    1) yes, we are using the AES-PZSDRCC-FMC-G board to program

    2) yes, it did power up on the Avnet carrier both before and after reprogramming the ADM1166

    3) 5.0 measures 5.08V and 3.3 measure 3.38

    4) we're running a custom image on SDCard, but the SOM boots fine on the FMC Carrier.  On custom carrier, PG_MODULE LED (D3) blinks constantly and VIN_EN never turns Q13 on.

    5) static bag says revC

     

    Thanks!