Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio What if I want a baremetal?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 357 subscribers
  • Views 308 views
  • Users 0 members are here
Related

What if I want a baremetal?

yahniukov
yahniukov over 9 years ago

The most examples for working with PicoZedTm SDR SOM Z7035/AD9361 Development Kit use the Linux or Matlab across Linux. But I want a baremetal solution.


My task is:

1. Send number from Host PC to Picozed using UART;

2. On Picozed send this number to DAC for transmit;

3. Then receive and read ADC and get the same number;

4. Send number to Host PC


HDL design I took here: https://github.com/analogdevicesinc/hdl/tree/master/projects/pzsdr/ccfmc


AD9361 API took here: https://github.com/analogdevicesinc/no-OS/tree/master/ad9361

Here I launched 'create_xilinx_sdk_project.bat' and got Xilinx SDK project.


And what is next? In 'dac_core.c' file I found 'void dac_write(struct ad9361_rf_phy *phy, uint32_t regAddr, uint32_t data)' method. It's how this method do writing data to DAC:

Xil_Out32(AD9361_TX_0_BASEADDR + regAddr, data);

What regAddr I need to transmit my data?  Obviously I have to see DAC Register Map. That's what I found: https://wiki.analog.com/resources/fpga/docs/hdl/regmap

Many-many registers but where the one what I need?


Another example.

In SDK example:

    /* LO Control */
    2400000000UL,    //rx_synthesizer_frequency_hz *** adi,rx-synthesizer-frequency-hz
    2400000000UL,    //tx_synthesizer_frequency_hz *** adi,tx-synthesizer-frequency-hz


But when I do next:

    uint64_t data = 0;
    ad9361_get_rx_lo_freq(ad9361_phy, &data);
    printf("%u \n", data);

I'm getting (Hz):

   1311496


WHY? What is going on?


May somebody can help me please? I need something like simple example code for  PicoZedTm SDR SOM Z7035/AD9361 that's working fine.

 

If I took wrong HDL design or something like this, get me please relevance links to right materials for PicoZedTm SDR SOM Z7035/AD9361