Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio PZSDR FMC carrier Eth PHY reset
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 357 subscribers
  • Views 253 views
  • Users 0 members are here
Related

PZSDR FMC carrier Eth PHY reset

e14 Contributor
e14 Contributor over 9 years ago
A couple of questions about the PZSDR FMC carrier Ethernet PHY reset.
 
The PZSDR FMC carrier drives the Ethernet PHY RESETN signal from a SN74LVC1G08 (2-bit AND) at U10 powered by 3.3v. The AND inputs are PG_MODULE (through an RC filter) and ETH1_RESETN. PG_MODULE is pulled up to VIN (nominally 5v) by the PZSDR SOM. The SN74LVC1G08 permits Vin up to 5.5v, so this seems ok. ETH1_RESETN is driven by the SOM at JX4.100. On the SOM JX4.100 is tied to Zynq pin B20 / MIO[51] in bank 501 with VDDO=1.8v.

 

Doesn't the 3.3v output of the SN74LVC1G08 exceed the absolute max voltage for the Marvell 88E1512 RESETN pin? The datasheet lists abs max of VDDO+0.7 for pins powered by VDDO; I think this includes RESETN.

 

The Zynq MIO[51] signal at 1.8v is below V_IH(min)=2.0v for the SN74LVC1G08 when VCC=3.3v. How does the Zynq reliably de-assert reset for the carrier's Eth PHY?