Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio PicoZed Questions
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 360 subscribers
  • Views 1763 views
  • Users 0 members are here
Related

PicoZed Questions

e14 Contributor
e14 Contributor over 10 years ago

We plan on using the PicoZed kit:

http://www.xilinx.com/products/boards-and-kits/1-au200Bskjht.html



1) It shows that the band is 70MHz to 6GHz.  We were wondering if the kit is ever run up to 6GHz or rather, is it practical.  What's the typical operating range?  



2) I got the user's manual 1.2 and near the end it states that the datasheet uses narrowband baluns while the test uses wideband baluns for the PicoZed SDR Z7035/AD9361.  Is it confirmed that this model uses wideband baluns (or both)?



3) Where can we find a footprint of the chip?  I don't think the manual has a clear one.



Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 8 years ago +1
    Hello, 1. For the PicoZed SOM, the only Carrier Card we hvae available that oprates with it is the PicoZed FMC V2. However, this does not prevent you from making your own custom carrier card. The PicoZed…
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello,

    1. For the PicoZed SOM, the only Carrier Card we hvae available that oprates with it is the PicoZed FMC V2. However, this does not prevent you from making your own custom carrier card. The PicoZed SOM requires a Carrier Card to operate.

    2. For information on LEDs and switches please refer to the Hardware User Guide on the FMC V2 Carrier http://zedboard.org/support/documentation/13076

    3. The PicoZed can be used for General Zynq 7000 All Programmable SoC prototyping. It is not application specific. However please verify it meets all your needs before purchasing be refering to the Hardware User Guide for both the SOM and Carrier Card

    4. The PicoZed FMC V2 Carrier Card has User Leds and push buttons. Please refer to the FMC V2 Carrier Card HW User Guide.

    5.System on Module(SOM) or  - This is refering to the module that plugs onto the carrier card. This SOM Guide goes into further details http://zedboard.org/content/design-it-or-buy-it

    System on Chip(SoC) - This is refering to the Zynq device that has both Programmable Logic and the Processing System in single device

    6. Please refer to this Post for information about the XADC on PicoZed http://zedboard.org/content/xadc-vp-vn-pin

    --Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello,

    1. For the PicoZed SOM, the only Carrier Card we hvae available that oprates with it is the PicoZed FMC V2. However, this does not prevent you from making your own custom carrier card. The PicoZed SOM requires a Carrier Card to operate.

    2. For information on LEDs and switches please refer to the Hardware User Guide on the FMC V2 Carrier http://zedboard.org/support/documentation/13076

    3. The PicoZed can be used for General Zynq 7000 All Programmable SoC prototyping. It is not application specific. However please verify it meets all your needs before purchasing be refering to the Hardware User Guide for both the SOM and Carrier Card

    4. The PicoZed FMC V2 Carrier Card has User Leds and push buttons. Please refer to the FMC V2 Carrier Card HW User Guide.

    5.System on Module(SOM) or  - This is refering to the module that plugs onto the carrier card. This SOM Guide goes into further details http://zedboard.org/content/design-it-or-buy-it

    System on Chip(SoC) - This is refering to the Zynq device that has both Programmable Logic and the Processing System in single device

    6. Please refer to this Post for information about the XADC on PicoZed http://zedboard.org/content/xadc-vp-vn-pin

    --Josh