Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio Board definition file for Vivado
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 360 subscribers
  • Views 1353 views
  • Users 0 members are here
Related

Board definition file for Vivado

e14 Contributor
e14 Contributor over 10 years ago

Good evening- where can I find the board definition file for PicoZed SDR to use with Vivado?

thank you

philip

  • Sign in to reply
  • Cancel
  • mbrown
    0 mbrown over 10 years ago

    We do not currently have Vivado Board Definition Files for PicoZed SDR.

    We do have TCL scripts for setting up the PS7 for everything hardwired on the SOM. The scripts sets up PS7 peripherals, DDR3L trace delays, clock/PLL settings, etc. for the SOM only (no carrier peripherals).

    There are also PS7 customization scripts for our carriers. All of this is available on the Analog Devices GitHub repository, where they keep all source code for their PicoZed SDR reference design.

    https://github.com/analogdevicesinc/hdl

     

    For example, below you can see the master (common) scripts for the SOM:

     

    image

     

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to mbrown

    Hi Matt,

    I have the PicoZed SDR dev kit and I am getting the below error when running the ADI TCL scripts for the PicoZed SDR:

    # adi_project_create ccfmc_pzsdr
    WARNING: [Device 21-436] No parts matched 'xc7z035ifbg676-2L'
    ERROR: [Coretcl 2-106] Specified part could not be found.
    INFO: [Common 17-206] Exiting Vivado at Tue Oct 11 17:04:27 2016...
     
    It seems that Vivado does not have the XC7035 part used on the PicoZed SDR. How do I make that part known to Vivado?
     
    Many thanks!
    Logan
     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Idsorenson,

    By chance are you using Vivado WebPack? Vivado WebPack only supports Zynq 7010 - 7030 devices. Refer to link below, page 15.

    http://www.xilinx.com/support/documentation/sw_manuals/xilinx2015_4/ug973-vivado-release-notes-install-license.pdf

    Downloading the Vivado Design Suit should solve your issue.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to jafoste4

    Yes, thanks Josh, that was the issue.

    It looks like we need a full Vivado Design Suite to work with the PicoZed SDR? 

    It seems strange that the PicoZed SDR kit doesn't come with the device-locked voucher like other Avnet Zedboard/FPGA kits (or am I mistaken on that?).

    I am on an evaluation license for now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hell Idsorenson,

    Unfortunaly it does not come with a device-locked voucher. 

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vinaygb
    0 vinaygb over 9 years ago in reply to e14 Contributor

    Hi ldsorenson,

    How to run these tcl scripts ?

    Do we have to use VisualDSP++ ?

    And are these script files going to provide PicoZed 7035 SOM option in Vivado or these are to be used when PicoZed board is connected for online configuration ?