Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio picozed does not maintain static ip
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 760 views
  • Users 0 members are here
Related

picozed does not maintain static ip

e14 Contributor
e14 Contributor over 10 years ago

I connect picozed eth0 port to eth0 on linux host.

I open up Terminal in picozed GUI, and set static IP of picozed by doing:

sudo ifconfig eth0 192.168.3.2 netmask 255.255.255.0 and, using ifconfig, verify that eth0 was indeed set to .192.168.3.2.

I set Linux laptop ethernet port as:

sudo ifconfig eth0 192.168.3.3 netmask 255.255.255.0

From Linux machine:

ping 192.168.3.2

The ping is successful for about a minute or two, then I "Destination Host Unreachable".

I use ifconfig in the picozed terminal, and eth0 is no longer set to 192.168.3.2.

All this is repeatable.  It seems the picozed is not holding its static ip assignment.  If that's the case, how to I get this to work with Matlab, which is expecting picozed to have that static ip?

Thanks -- Jeff

  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 10 years ago

    Hi Jeff.  Try this to stop the service from releasing the IP address according to DHCP timouts:

     

    stop network-manager

     

    Works for me.

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to mbrown

    Works for me too.  Thanks Matt.  I suppose I should let Mathworks know about this, their documentation for PicoZed does address this issue at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mbrown
    0 mbrown over 10 years ago in reply to e14 Contributor

    Thanks Jeff. I'll get in touch with MathWorks. We work closely with them.

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mbrown
    0 mbrown over 10 years ago in reply to mbrown

    Just to close this one off, the issue here is that to use the MathWorks flow you need to use their Linux image. In that case, there's no need to stop the DHCP network manager.

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mbrown
    0 mbrown over 10 years ago in reply to mbrown

    Just to close this one off, the issue here is that to use the MathWorks flow you need to use their Linux image. In that case, there's no need to stop the DHCP network manager.

    /Matt