Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio PicoZed SDR power-only carrier
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 359 subscribers
  • Views 1945 views
  • Users 0 members are here
Related

PicoZed SDR power-only carrier

liuf_stanford
liuf_stanford over 9 years ago

We're developing an application using the PicoZed SDR which needs only power inputs from the carrier - no IO (ethernet, USB, HDMI, etc...) required. Since we don't want to re-invent the wheel, are there any such designs which already implement this functionality? If not, are there any good resources out there which might help us design our own carrier?

 

I know Avnet no longer sells PicoZed SDR units, but I'm posting here since replies on the EngineerZone forum are slow (and mostly useless).

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    I'm not aware of a power only carrier... the most minimal carrier available that I know of is the breakout carrier: http://zedboard.org/product/picozed-sdr-breakout-carrier .  But, if you really just need power, you could install a power connector by soldering wires directly to the PicoZed SDR module (be sure to strain relief the wire, looping it through a mounting hole or something, so it doesn't rip the pads from the board if it gets pulled on).  It wouldn't take much to throw together a simple PCB to provide just +5V to one of the connectors either (if you can solder one of the mating surface mount connectors).

     

    Also... IIRC, it needs an updated power sequencer load to run from only +5V.  Otherwise, the module won't boot while it waits for the rest of the voltages.

     

    Pat

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    I'm not aware of a power only carrier... the most minimal carrier available that I know of is the breakout carrier: http://zedboard.org/product/picozed-sdr-breakout-carrier .  But, if you really just need power, you could install a power connector by soldering wires directly to the PicoZed SDR module (be sure to strain relief the wire, looping it through a mounting hole or something, so it doesn't rip the pads from the board if it gets pulled on).  It wouldn't take much to throw together a simple PCB to provide just +5V to one of the connectors either (if you can solder one of the mating surface mount connectors).

     

    Also... IIRC, it needs an updated power sequencer load to run from only +5V.  Otherwise, the module won't boot while it waits for the rest of the voltages.

     

    Pat

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer