Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio Console setting in initramfs
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 556 views
  • Users 0 members are here
Related

Console setting in initramfs

e14 Contributor
e14 Contributor over 10 years ago
I'm in the process of porting the embedded system for a picozed-based platform from the Xilinx-v2013.4 (3.12 kernel) to the Xilinx-v2016.2 (4.4 kernel). The former version still makes use of an initial RAM disk (initrd) while the new uses an initial RAM fs (initramfs).
 
At boot time, the console is given through the serial interface on the USB connector. I expect it to be ttyPS0. At this point already, I don't know how this relation 'console-ttyPS0' is done !? Does it come from the device tree (I don't see any thing mentioning ttyPS0) ? In the former version (in the RAM disk), it was even not configured in the "init" scripts, neither in 'mdev' configuration file.

 

The boot process is running and then it hangs. Here is the output :

 

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Booting Linux on physical CPU 0x0
Linux version 4.4.0-test (pierrett@build0109-linux) (gcc version 4.8.3 20140320 (prerelease) (Sourcery CodeBench Lite 2014.05-23) ) #1 SMP PREEMPT Thu Aug 18 12:10:52 CEST 2016
CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: zynq
bootconsole [earlycon0] enabled
cma: Reserved 16 MiB at 0x3dc00000
Memory policy: Data cache writealloc
PERCPU: Embedded 12 pages/cpu @ef7d2000 s18240 r8192 d22720 u49152
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260608
Kernel command line: bootargs=console=ttyPS0,115200 root=/dev/ram initrd=0x8000000 rw earlyprintk rootwait
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1009532K/1048576K available (4456K kernel code, 213K rwdata, 1564K rodata, 240K init, 193K bss, 22660K reserved, 16384K cma-reserved, 238976K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)
    lowmem  : 0xc0000000 - 0xf0000000   ( 768 MB)
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)
      .text : 0xc0008000 - 0xc05e949c   (6022 kB)
      .init : 0xc05ea000 - 0xc0626000   ( 240 kB)
      .data : 0xc0626000 - 0xc065b450   ( 214 kB)
       .bss : 0xc065b450 - 0xc068bb54   ( 194 kB)
Preemptible hierarchical RCU implementation.
        Build-time adjustment of leaf fanout to 32.
        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=2
NR_IRQS:16 nr_irqs:16 16
ps7-slcr mapped to f0802000
L2C: platform modifies aux control register: 0x72360000 -> 0x72760000
L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000
L2C-310 erratum 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 1 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 8 ways, 512 kB
L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001
zynq_clock_init: clkc starts at f0802100
Zynq clock init
sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns
clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns
clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns
ps7-ttc #0 at f080a000, irq=18
Console: colour dummy device 80x30
console [tty0] enabled
bootconsole [earlycon0] disabled

 

My feeling is that the trouble comes from a wrong setting of the console. In the boot log, one can notice that the "tty0" is enabled while in the boot arguments, I expect the console on ttyPS0.

 

Could any one explain how the correct console could be set at startup ?

Many thanks in advance

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 10 years ago

    Hello Tpierret,

    Porting any system from 3.12 to 4.4 is a monumental task, and likely is only ging to be the first of many issues. A better approach is to start with 4.4 Kernel that works properly on your hardware, then port the components that comprise the custom system to that. Otherwise, each problem will require either prior knowledge from someone who has solved the same issue before, or a deep dive into kernel differences which can be extremely time consuming.

    -- Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jafoste4

    Hi Josh,

    Thanks for the answer.

    I do not really understand what you mean with "start with a 4.4 kernel that works properly". This is indeed my goal. My starting point is a properly working  3.12 kernel.

    Unfortunately I cannot compile the latest PetaLinux kernel as a reference. None of my computers gather the mandatory prerequisites.

    I already did a big job of updating the configuration in a test/error process. I think I'm now close to the goal, but blocked anyway :-(

    Regards.

    Thierry