Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio Can't connect Matlab to PicoZed SDR
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 823 views
  • Users 0 members are here
Related

Can't connect Matlab to PicoZed SDR

e14 Contributor
e14 Contributor over 10 years ago

I'm able to ping Picozed from Terminal on Linux laptop.

PicoZed is on 192.168.3.2
Laptop is on 192.168.3.3

Then I start MATLAB on Linux laptop.  I follow instructions in Matlab documentation  for "Manual Host-Radio Hardware Setup".  In "Step 3", I successfully do:
dev = sdrdev('PicoZed SDR');
setupSession(dev);

Then, I go to "Step 8" and get a warning and error when I do:
i = info(dev)

And I also get an error when I do:
setAddress(dev, 'IP Address', '192.168.3.2');

I tried to upload a Matlab screenshot to:

http://picozed.org/imce?app=ckeditor%7Csendto%40ckeditor_imceSendTo%7C&CKEditor=edit-body-und-0-value&CKEditorFuncNum=2&langCode=en

  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 10 years ago

    Are you connected to a DHCP enabled switch/router, or assigning a static IP?

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to mbrown

    Using static IP,  addresses as listed above.  Matlab docs specify that a direct connection should be made (i.e., no other network equipment involved) and static IPs be used with above addresses.  So that's what i did.

    Thanks -- jeff 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to mbrown

    Using static IP,  addresses as listed above.  Matlab docs specify that a direct connection should be made (i.e., no other network equipment involved) and static IPs be used with above addresses.  So that's what i did.

    Thanks -- jeff