Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio AD9361 Sample Rate
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 1285 views
  • Users 0 members are here
Related

AD9361 Sample Rate

yahniukov
yahniukov over 9 years ago

I have PicoZedTm SDR SOM Z7035/AD9361 Development Kit.

 

On the repository https://github.com/analogdevicesinc/libiio in examples I found ad9361-iiostream.c.

 

In this file author set sample rate 2.5 MS/s for rx and tx.

 

In datasheets I did not found information about recommended sample rate for AD9361.

 

Can somebody help me to know what is recommended sample rate for AD9361?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 9 years ago +1 verified
    The sample rate depends on your specific needs. In the case of Rx, a lower sample rate will produce less data, which will require less storage, processing, etc. But it will also "see" less bandwidth. So…
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    The sample rate depends on your specific needs.  In the case of Rx, a lower sample rate will produce less data, which will require less storage, processing, etc.  But it will also "see" less bandwidth.  So, if you're looking for a signal that's 1 MHz wide, 2.5MS/s will be fine.  But if you're looking for a signal that's 10 MHz wide, 2.5MS/s won't be enough.  Since they're complex samples, 2.5MS/s will give you 2.5 MHz of bandwidth, though the outer edges will begin to roll off, so I'd recommend sampling at least a little bit higher than the bandwidth you need.

     

    If you're not familiar with the theory, you should read up on sampling, Nyquist, etc.

     

    Pat

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    The sample rate depends on your specific needs.  In the case of Rx, a lower sample rate will produce less data, which will require less storage, processing, etc.  But it will also "see" less bandwidth.  So, if you're looking for a signal that's 1 MHz wide, 2.5MS/s will be fine.  But if you're looking for a signal that's 10 MHz wide, 2.5MS/s won't be enough.  Since they're complex samples, 2.5MS/s will give you 2.5 MHz of bandwidth, though the outer edges will begin to roll off, so I'd recommend sampling at least a little bit higher than the bandwidth you need.

     

    If you're not familiar with the theory, you should read up on sampling, Nyquist, etc.

     

    Pat

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • yahniukov
    0 yahniukov over 9 years ago in reply to e14 Contributor

    Thank you!